- Sat May 15, 2010 4:42 pm
#101035
Well, l i am trying to receive data from my LS0031 GPS module via UART communication using an avr ATtiny2313.
My thought is to receive data from the gps and sent it as it is, to an LCD HD44780 to watch them, as a first step. The problem i came across with is that i receive data and i see characters at the LCD but it isn't NMEA code. I can not see any ascii code like a $ start bit , or GPGGA or a whole sentense like $GPGGA,053740.000,2503.6319,N,12136.0099,E,1,08,1.1,63.8,M,15.2,M,,0000*64. What i see is different characters with ascii code like 0xA9 translated to chinesse chars or somethink like this, and sometimes i watch ascii like 0x43 which is real chars and seems like a part of NMEA code. Note that the chars i see at the LCD depends on the gps transmit. If i stop the transmit unplugging the transmits gps cable the chars i see at the lcd stops too.
I concluded that the problem is at the frames and how the avr translate and receive the transfered bytes.
I have checked the UART initialization thousands of times and i can't find any mistake.
I'll write below what i did with the avr and if anyone see something wrong or something helpfull please reply and help me.
Here we are:
MCU:ATtiny2313
External Oscillator for stable frequency at 4mhz
GPS works at default settings: 9600 bps, 8 data bits, no parity, 1 stop bits (default) as manual writes.
So the settings i set at the initialization is:
UCSRB: Set RXEN to enable Receiver
UCSRC: Set UCSZ0:1 for 8 data bits no parity and 1 stop bit.
UBRR=25 for a baud rate of 9600 with 0.2% error as Attiny2313 manual says.
The Source Code.
PS. Sorry for my English it isn't my native language and it takes me some time to explain you my problem in english.
I want to beleive that i made you understand my problem and somebody will help me.
My thought is to receive data from the gps and sent it as it is, to an LCD HD44780 to watch them, as a first step. The problem i came across with is that i receive data and i see characters at the LCD but it isn't NMEA code. I can not see any ascii code like a $ start bit , or GPGGA or a whole sentense like $GPGGA,053740.000,2503.6319,N,12136.0099,E,1,08,1.1,63.8,M,15.2,M,,0000*64. What i see is different characters with ascii code like 0xA9 translated to chinesse chars or somethink like this, and sometimes i watch ascii like 0x43 which is real chars and seems like a part of NMEA code. Note that the chars i see at the LCD depends on the gps transmit. If i stop the transmit unplugging the transmits gps cable the chars i see at the lcd stops too.
I concluded that the problem is at the frames and how the avr translate and receive the transfered bytes.
I have checked the UART initialization thousands of times and i can't find any mistake.
I'll write below what i did with the avr and if anyone see something wrong or something helpfull please reply and help me.
Here we are:
MCU:ATtiny2313
External Oscillator for stable frequency at 4mhz
GPS works at default settings: 9600 bps, 8 data bits, no parity, 1 stop bits (default) as manual writes.
So the settings i set at the initialization is:
UCSRB: Set RXEN to enable Receiver
UCSRC: Set UCSZ0:1 for 8 data bits no parity and 1 stop bit.
UBRR=25 for a baud rate of 9600 with 0.2% error as Attiny2313 manual says.
The Source Code.
Code: Select all
.NOLIST ; Don't list the following in the list file
.INCLUDE "tn2313def.inc" ; Import of the file
.LIST ; Switch list on again
.equ RS=5
.equ RW=6
.equ E=4
.def temp1= r16
.def temp2= r17
.cseg
.org 0
rjmp RESET
rjmp RESET
rjmp RESET
RESET:
;Init Stack Pointer
ldi temp1, low(RAMEND)
out spl, temp1
;Configure Pins
ldi temp1,0xFF
out DDRB, temp1
ldi temp1,0x71
out DDRD, temp1
;Wait fot LCD to boot
rcall wait_LCD
;Configure LCD
rcall init_LCD
;Configure USART
rcall init_USART
;Main program
main:
;Here I receive a data byte and i send it to LCD
rcall receive_USART
rcall write_LCD
;And a small delay here to have time to see the char at the lcd
rcall delay
rjmp main
;!--------------------------------USART--------------------------------!
;***********************************************
;************** Initialize USART ***************
;***********************************************
init_USART:
;Set Baud Rate 9600
ldi temp1,0
ldi temp2,25
out UBRRH,temp1
out UBRRL,temp2
;Enable Receive
ldi temp1,(1<<RXEN)
out UCSRB,temp1
;8-bit, no parity, 1 stop bit
ldi r16,(3<<UCSZ0)
out UCSRC,temp1
ret
;***********************************************
;************** Receive Dt USART ***************
;***********************************************
receive_USART:
;Wait for data to be received
sbis UCSRA,RXC
rjmp receive_USART
;Get and return received data from buffer
in temp1,UDR
ret
;!---------------------------------LCD---------------------------------!
;***********************************************
;**************** Initialize LCD ***************
;***********************************************
init_LCD:
;LCD Configuration
ldi temp1,0b00111000 ;8-bit, 2-lines, 5x8 dots
rcall command_LCD
ldi temp1,0b00001111 ;Display on, show Cursor, blink
rcall command_LCD
ldi temp1,0b00000110 ;cursor increament,No display shift
rcall command_LCD
ldi temp1,0x01 ;Return Home
rcall command_LCD
ret
;***********************************************
;*************** Commands to LCD ***************
;***********************************************
command_LCD:
sbi PORTD,E ;Set E
cbi PORTD,RW ;clear RW bit for writing
cbi PORTD,RS ;clear RS bit for commands
out PORTB,temp1
cbi PORTD,E
rcall wait_LCD
ret
;***********************************************
;***************** Write to LCD ****************
;***********************************************
write_LCD:
sbi PORTD,E ;Set E
cbi PORTD,RW ;Clear RW bit for writing
sbi PORTD,RS ;Set RS bit for data
out PORTB,temp1 ;Put data to data bus
cbi PORTD,E
rcall wait_LCD
ret
;***********************************************
;***************** Wait for LCD ****************
;***********************************************
wait_LCD:
sbi PORTD,RW ;turn in read mode busy flag
cbi PORTD,RS
ldi temp1,0x00 ;turn PortB input
out DDRB,r16
sbi PORTD,E ;take E high
nop
in temp2,PINB ;get address and busy flag
cbi PORTD,E
ldi temp1,0xFF ;turn PortB output again
out DDRB,r16
cbi PORTD,RW
sbrc temp2,7
rjmp wait_LCD
sbi PORTD,E
ret
;***********************************************
;****************** Delay Loop *****************
;***********************************************
delay:
; =============================
; delay loop generator
; 7000000 cycles:
; -----------------------------
; delaying 6999996 cycles:
ldi R20, $76
WGLOOP0: ldi R21, $75
WGLOOP1: ldi R22, $A8
WGLOOP2: dec R22
brne WGLOOP2
dec R21
brne WGLOOP1
dec R20
brne WGLOOP0
; -----------------------------
; delaying 3 cycles:
ldi R20, $01
WGLOOP3: dec R20
brne WGLOOP3
; -----------------------------
; delaying 1 cycle:
nop
; =============================
ret
PS. Sorry for my English it isn't my native language and it takes me some time to explain you my problem in english.
I want to beleive that i made you understand my problem and somebody will help me.