- Sat May 15, 2010 10:49 am
#101024
After a lot of hours... testing and writing code i did my LCD work! Because it was difficult for me to get it work, i thought that it would be a good idea, to share my code with you, who maybe trying to do the same think with me. Interface a HD44780 to an ATtiny2313. The source code is writen in assembly, it is tested and it works!. Copy it and test it yourself!
I use all PORTB pins for data bus and PORTD pins 4, 5, 6 for E, RS, RW
I use all PORTB pins for data bus and PORTD pins 4, 5, 6 for E, RS, RW
Code: Select all
.NOLIST ; Don't list the following in the list file
.INCLUDE "tn2313def.inc" ; Import of the file
.LIST ; Switch list on again
.equ E=4
.equ RS=5
.equ RW=6
.def temp1= r16
.def temp2= r17
.cseg
.org 0
rjmp RESET
rjmp RESET
rjmp RESET
RESET:
;Init Stack Pointer
ldi r16, low(RAMEND)
out spl, temp1
;Configure Pins
ldi temp1,0xFF
out DDRB, temp1
ldi temp1,0x71
out DDRD, temp1
;Wait for LCD to boot
rcall wait_LCD
;Configure LCD
rcall init_LCD
;Write Char A to LCD
ldi temp1,'A'
rcall write_LCD
;Main program
main:
nop
rjmp main
;***********************************************
;**************** Initialize LCD ***************
;***********************************************
init_LCD:
ldi temp1,0b00111000 ;8-bit, 2-lines, 5x8 dots
rcall command_LCD
ldi temp1,0b00001111 ;Display on, show Cursor, blink
rcall command_LCD
ldi temp1,0b00000110 ;cursor increament, No display shift
rcall command_LCD
ldi temp1,0x01 ;Return Home
rcall command_LCD
ret
;***********************************************
;*************** Commands to LCD *************
;***********************************************
command_LCD:
sbi PORTD,E ;Set E
cbi PORTD,RW ;clear RW bit for write mode
cbi PORTD,RS ;clear RS bit for command mode
out PORTB,temp1
cbi PORTD,E
rcall wait_LCD
ret
;***********************************************
;***************** Write to LCD ****************
;***********************************************
write_LCD:
sbi PORTD,E ;Set E
cbi PORTD,RW ;Clear RW bit for writing
sbi PORTD,RS ;Set RS bit for data
out PORTB,temp1 ;Put data to data bus
cbi PORTD,E
rcall wait_LCD
ret
;***********************************************
;***************** Wait for LCD ****************
;***********************************************
wait_LCD:
sbi PORTD,RW ;turn in read mode busy flag
cbi PORTD,RS
ldi temp1,0x00 ;turn PortB input
out DDRB,r16
sbi PORTD,E ;take E high
nop
in temp2,PINB ;get address and busy flag
cbi PORTD,E
ldi temp1,0xFF ;turn PortB output again
out DDRB,r16
cbi PORTD,RW
sbrc temp2,7
rjmp wait_LCD
sbi PORTD,E
ret