- Sun Nov 22, 2009 7:05 am
#85627
Hi,
i have connected a Nintendo DS TouchScreen to my Arduino duemilanove and i'm able to get only the x axis value, while the Y value is always 0 (zero).
Naturally i have read a lot of stuff on the web and tried a lot of scripts and connections (i'm not so good in electronic stuff so I often get inspiration from web) and it seems other people had the same problems (for example on this post: viewtopic.php?t=16873&highlight=touch+screen+nintendo)
Following the last source code I used :
Connections
I used four 10K Resistor connecting every pin to ground
A0 --> x1
A1 --> y2
A2 --> x2
A3 --> y1
Thanks in advance
Fabio
i have connected a Nintendo DS TouchScreen to my Arduino duemilanove and i'm able to get only the x axis value, while the Y value is always 0 (zero).
Naturally i have read a lot of stuff on the web and tried a lot of scripts and connections (i'm not so good in electronic stuff so I often get inspiration from web) and it seems other people had the same problems (for example on this post: viewtopic.php?t=16873&highlight=touch+screen+nintendo)
Following the last source code I used :
Code: Select all
//modified to match my sparkfun connector
#define xLow 17
#define xHigh 15
#define yLow 16
#define yHigh 14
void setup(){
Serial.begin(9600);
}
void loop(){
pinMode(xLow,OUTPUT);
pinMode(xHigh,OUTPUT);
digitalWrite(xLow,LOW);
digitalWrite(xHigh,HIGH);
digitalWrite(yLow,LOW);
digitalWrite(yHigh,LOW);
pinMode(yLow,INPUT);
pinMode(yHigh,INPUT);
delay(10);
//xLow has analog port -14 !!
int x=analogRead(yLow -14);
pinMode(yLow,OUTPUT);
pinMode(yHigh,OUTPUT);
digitalWrite(yLow,LOW);
digitalWrite(yHigh,HIGH);
digitalWrite(xLow,LOW);
digitalWrite(xHigh,LOW);
pinMode(xLow,INPUT);
pinMode(xHigh,INPUT);
delay(10);
//xLow has analog port -14 !!
int y=analogRead(xLow - 14);
Serial.print(x,DEC);
Serial.print(",");
Serial.println(y,DEC);
delay(200);
}
Connections
I used four 10K Resistor connecting every pin to ground
A0 --> x1
A1 --> y2
A2 --> x2
A3 --> y1
Thanks in advance
Fabio