- Fri Oct 09, 2009 12:12 pm
#82696
I am working on a RFID reader using the ID-20. It outputs serial data in the following format. Each [] is one ascii byte.
[STX]
[D1] [D2] [D3] [D4] [D5] [D6] [D7] [D8] [D9] [D10]
[CS1] [CS2]
[CR]
[LF]
[ETX]
The part I care about is the D1-D10, the actual data, 10 ascii charactors. CS1 and CS2 are 2 ascii charactors that are the checksum for the data. I would like to implement checking the data against the check sum but I cant seem to convert the charactors into the format I need. Here is how the data sheet says the checksum is done to the data
if the 10 digits of ascii come in and lets say they equal
2 4 0 0 C C 5 7 8 3
and the check sum is
3 C
then to get the checksum you need to take pairs of ascii and convert them into one HEX byte and then XOR the hex bytes. which would look like this.
2 4 0 0 C C 5 7 8 3
becomes
[24] [00] [CC] [57] [83]
and 3 C becomes [3C]
then you can do a simple [24] ^ [00] ^ [CC] ^ [57] ^ [83] (^ is XOR) to see if it = [3C]
The problem I am having is I dont know how to convert 10 ascii bytes into 5 pairs of 2 HEX bytes.
again... here is what I need to do (brackets [] used to illustrate seperate bytes)
ASCII [a] [c] [d] [e] [f]
HEX [ab] [cd] [ef]
Here is a piece of sample code that is not working that is attempting to do this
[STX]
[D1] [D2] [D3] [D4] [D5] [D6] [D7] [D8] [D9] [D10]
[CS1] [CS2]
[CR]
[LF]
[ETX]
The part I care about is the D1-D10, the actual data, 10 ascii charactors. CS1 and CS2 are 2 ascii charactors that are the checksum for the data. I would like to implement checking the data against the check sum but I cant seem to convert the charactors into the format I need. Here is how the data sheet says the checksum is done to the data
if the 10 digits of ascii come in and lets say they equal
2 4 0 0 C C 5 7 8 3
and the check sum is
3 C
then to get the checksum you need to take pairs of ascii and convert them into one HEX byte and then XOR the hex bytes. which would look like this.
2 4 0 0 C C 5 7 8 3
becomes
[24] [00] [CC] [57] [83]
and 3 C becomes [3C]
then you can do a simple [24] ^ [00] ^ [CC] ^ [57] ^ [83] (^ is XOR) to see if it = [3C]
The problem I am having is I dont know how to convert 10 ascii bytes into 5 pairs of 2 HEX bytes.
again... here is what I need to do (brackets [] used to illustrate seperate bytes)
ASCII [a] [c] [d] [e] [f]
HEX [ab] [cd] [ef]
Here is a piece of sample code that is not working that is attempting to do this
Code: Select all
I found a link to someone who did this in assembly language but I am trying to do it on an arduino so the codes not even close. Anyone know how to do this?int count = 0;
for ( int i = 0; i < 10; i+=2 )
{
hex[count] = data[i]+data [i+1];
count++;
}
www.pcmofo.com