SparkFun Forums 

Where electronics enthusiasts find answers.

Your source for all things Atmel.
By shawc01
#82073
Hi,

I want to send an audio stream over bluetooth to multiple recievers. Catch is I want to do this as cheap as possible.

I was wondering whether I can use a cheap bluetooth dongle connected to a USB enabled AVR and send the audio over bluetooth that way?

I won't go into too much more detail until someone can confirm whether this will be possible at all.

Cheers
By MichaelN
#82075
Well, the USB AVR chips can operate in host mode, so in theory it would be possible. In practice, it might take a LOT of work to write the AVR drivers for the dongle, unless the protocol has been published or someone else has already figured out how to do it with that particular dongle.

I would have thought you'd be best to use a bluetooth module designed for embedded use, that has code already written you can use. Sparkfun has them starting from $35. There would be much cheaper options once you start talking about high volumes.

A $10 dongle won't seem such good value if you spend weeks or months trying to get it working.
By Dutch2
#82086
The Bluegiga WT32 works great for audio. You can configure it through a simple serial port protocol so it's easy to connect to a micro.

Not sure about multiple connections... what mode do you want to use?

D2.
By tz
#83630
Non-USB bluetooth dongles tend to be expensive

There is a difference between one to 2-3, or to 10 or 100.

Bluetooth sound profiles are 1 to 1.

The headphone/handsfree and the A2DP are both computationally intensive (think MP3) - they don't just send an 8 bit sample stream.

So it probably is NOT possible, at least not knowing more details.
By tz
#84175
There are two algorithms, one faster but (relatively) low quality for headsets HSP, and a high quality for music, A2DP. They are lossy compression much like MP3. The bluez stack for linux implements both (at least in beta) and it is open source.

It is NOT a voltage level. It is a set of frequencies put through a compressor.