I have it hooked up to ports 50-53 and INT0 (D2) and am using the code supplied in the thread http://www.arduino.cc/cgi-bin/yabb2/YaB ... 4359/59#59 over at arduino.cc.
As you can see described in that post from myself, I can get video pass-through working fine - I jsut can't generate any OSD and the module seems to loose sync regularly untill you touch near the GND pin on the connector block.
I dont have any pullups or other hardware - just the breakout going to a breadboard going to the pins on the arduino. From what I could makeout from the Schematics, everything is onboard and I should be able to generate an OSD by now!!

Any tips or suggestions from anyone that has used this board succesfully would be *massively* appreciated.
Thanks in advance!
Adrian