- Thu Feb 19, 2009 9:29 pm
#66735
I'm having a problem calling a function multiple times when the same parameters are passed to it. I am using AtTiny24 with AVR Studio 4.15 build 623. The function will work correctly the first time and again as long as the parameters passed to it are different. For example my WriteLcd() function, if I do
WriteLcd("MSG",3); //works fine
WriteLcd("MSG1",4); //Works fine
WriteLcd("MSG",3); //Stops Working and prints // to the LCD
WriteLcd("MSG2",4); //Works fine
WriteLcd("MSG2",4); //Stops Working and prints // to the LCD
Like wise if I do
WriteLcd(string,strlen(string)); //Works fine
WriteLcd(string,strlen(string)); //Stops Working and prints // to the LCD
I have tried setting different optimizations with no luck. Any help would be appreciated.
WriteLcd("MSG",3); //works fine
WriteLcd("MSG1",4); //Works fine
WriteLcd("MSG",3); //Stops Working and prints // to the LCD
WriteLcd("MSG2",4); //Works fine
WriteLcd("MSG2",4); //Stops Working and prints // to the LCD
Like wise if I do
WriteLcd(string,strlen(string)); //Works fine
WriteLcd(string,strlen(string)); //Stops Working and prints // to the LCD
I have tried setting different optimizations with no luck. Any help would be appreciated.
Code: Select all
#define F_CPU 8000000UL
#include <avr/io.h>
#include <util/delay.h>
// LCD is connected to PA0
#define LCDPIN 0
// Button is connected to PA1
#define BTNPIN 1
//Write string to LCD at 9600 baud
void WriteLcd(char *string,int len);
void WriteLcd(char *string,int len)
{
int bitloop,charloop;
for(charloop=0;charloop<len;charloop++)
{
PORTA&=~(_BV(LCDPIN)); //Start Signal
_delay_us(104);
for(bitloop=0;bitloop<8;bitloop++)
{
if(string[charloop]&0x01)
{
PORTA |= _BV(LCDPIN);
}
else
{
PORTA&=~(_BV(LCDPIN));
}
string[charloop]>>=1;
_delay_us(104);
}
PORTA |= _BV(LCDPIN); //Stop Signal
_delay_us(104);
}
}
int main(void)
{
DDRA=0xFD; // Pin A1 input, others output
PORTA = 0x03; // Enable internal pull-up resistor on PA1 and set others low
char string[]="Hello";
_delay_ms(300);
WriteLcd("HI",2); //prints fine
WriteLcd("HI",2); //prints garbage
while(1)
{
if(bit_is_clear(PINA, BTNPIN))
{
WriteLcd(string,6);
while(bit_is_clear(PINA, BTNPIN));
}
}
return 0;
}