- Tue Jun 10, 2008 12:57 pm
#50008
I want to print out the angle in degreese, like 43.1 from this module http://www.sparkfun.com/commerce/produc ... cts_id=761
at the moment it prints out this rotating an whole round when its connected to 5v:
Direction 1: 75
Direction 2: 113
Direction 1: 76
Direction 2: 116
Direction 1: 76
Direction 2: 116
Direction 1: 76
Direction 2: 112
Direction 1: 74
Direction 2: 114
Direction 1: 77
Direction 2: 110
Direction 1: 76
Direction 2: 116
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
3volt gives this
Direction 1: 312
Direction 2: 300
Direction 1: 312
Direction 2: 300
Direction 1: 312
Direction 2: 300
Direction 1: 311
Direction 2: 300
Direction 1: 311
Direction 2: 300
at the moment it prints out this rotating an whole round when its connected to 5v:
Direction 1: 75
Direction 2: 113
Direction 1: 76
Direction 2: 116
Direction 1: 76
Direction 2: 116
Direction 1: 76
Direction 2: 112
Direction 1: 74
Direction 2: 114
Direction 1: 77
Direction 2: 110
Direction 1: 76
Direction 2: 116
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
Direction 1: 77
Direction 2: 117
3volt gives this
Direction 1: 312
Direction 2: 300
Direction 1: 312
Direction 2: 300
Direction 1: 312
Direction 2: 300
Direction 1: 311
Direction 2: 300
Direction 1: 311
Direction 2: 300
Code: Select all
/*
* Smoothing
* David A. Mellis <dam@mellis.org>
*
* Reads repeatedly from an analog input, calculating a running average
* and printing it to the computer.
*
* http://www.arduino.cc/en/Tutorial/Smoothing
*/
// Define the number of samples to keep track of. The higher the number,
// the more the readings will be smoothed, but the slower the output will
// respond to the input. Using a #define rather than a normal variable lets
// use this value to determine the size of the readings array.
#define NUMREADINGS 10
#define dir1 0
#define dir2 1
long previousMillis = 0; // will store last time LED was updated
long interval = 3000; // interval at which to blink (milliseconds)
int readings[NUMREADINGS][5]; // the readings from the analog input
int index = 0; // the index of the current reading
int total1,total2,direction1,direction2;
void setup()
{
Serial.begin(9600);
Serial.println("No stratet serieporten"); // initialize serial communication with computer
pinMode(2, OUTPUT);
digitalWrite(2,HIGH);
delay(2000);
digitalWrite(2,LOW);
total1 = 0;
total2 = 0;
}
void loop()
{
total1 +=analogRead(dir1); // add the reading to the total
total2 += analogRead(dir2); // add the reading to the total
index++; // advance to the next index
if (index >= NUMREADINGS) { // if we're at the end of the array...
index = 0; // ...wrap around to the beginning
direction1 = total1 / NUMREADINGS; // calculate the average
direction2 = total2 / NUMREADINGS; // calculate the average
total1 = 0;
total2 = 0;
}
if (millis() - previousMillis > interval) {
previousMillis = millis(); // remember the last time we blinked the LED
Serial.print("Direction 1: ");
Serial.println(direction1); // send it to the computer (as ASCII digits)
Serial.print("Direction 2: ");
Serial.println(direction2); // send it to the computer (as ASCII digits)
}
}