Attiny45 Pin State on Power Up

Discussions on the software and hardware for Atmel's STK standard.

Moderator: phalanx

Post Reply
nvxwax
Posts: 3
Joined: Mon Oct 20, 2014 10:50 am

Attiny45 Pin State on Power Up

Post by nvxwax » Mon Oct 20, 2014 11:25 am

What is the pin state during power up, Im using an ATtiny45 to control a few relays and when powered up it turns them on for a short time, once everything is settled everything runs fine, they are being controlled via pulse width from a RC radio, is there a way to force the output pins to stay high or low during power up?

Thanks

User avatar
leon_heller
Support Volunteer
Posts: 5734
Joined: Sun May 01, 2005 11:20 am
Location: St. Leonards-on-Sea, E. Sussex, UK.

Re: Attiny45 Pin State on Power Up

Post by leon_heller » Mon Oct 20, 2014 2:33 pm

I/O pins are tri-stated on reset. You will have to pull them up or down with resistors if you want them to have a known value on power up.
Leon Heller
G1HSM

nvxwax
Posts: 3
Joined: Mon Oct 20, 2014 10:50 am

Re: Attiny45 Pin State on Power Up

Post by nvxwax » Mon Oct 20, 2014 5:25 pm

I pull them low to control the relays, how and what resistor would I use to keep them high on reset?

jremington
Support Volunteer
Posts: 2103
Joined: Fri Jun 15, 2007 9:41 pm
Location: Eugene, Or

Re: Attiny45 Pin State on Power Up

Post by jremington » Mon Oct 20, 2014 5:43 pm

100K to Vdd on each input pin should work well.

nvxwax
Posts: 3
Joined: Mon Oct 20, 2014 10:50 am

Re: Attiny45 Pin State on Power Up

Post by nvxwax » Mon Oct 20, 2014 6:05 pm

Thanks, I'm kinda new to all of this, it's nice not to get such help for a simple question lol

Post Reply