- Fri Feb 07, 2014 5:53 am
#168157
I have a task transmit stream ~4MBit from device to PC. LUFA use 'superloop', because i think it can be slow.
Most application use CDC/HID/Masstorgae - I can't use it. Board is ok - I have tested it with LUFA demos.
The Truble is that MCU dont' interrupt when it recieved SETUP packet. Source should be UEINTX.RXSTPI, UEIENX.RXSTPE, , sei() enabled.
I made 'debugger' -output info on UART. What I see?
MCU caught USB General Interrupt as source bus reset and USB Endpoint Interrupt _only_ with UEINTX.TXINI.
I connected logic analiser - it showed that host sended DeviceDescriptor, but MCU didn't catch it.
I read datashet lot of times, + USB NutShell + particulary USB specification.
One more moment - I mean, MCU shoul recive 'body' DevDecsr request, but where It should be? UEBCLX always is 0.
I haven't any ideas.
"debugger" sends: R 08: 21 00 00: 00 18 00: 00 18 00: 00 18 00: 00 18 00: 00 18 00
R 08 - isn't wrong, you can find comented line.
R - reset, USB not initialized .
08 - reg. UEIENX before sei()
: 21 00 00 - UECONX and, copied from interrupt UDINT and UEINTX. UECONX.STALLRQ - Cleared by hardware when a new SETUP is received.(my small test)
: 00 18 00 - the same next times.
* - didn't print, ENDPOINT interrupt not called
Source code - bellow. Then - analiser report.
Most application use CDC/HID/Masstorgae - I can't use it. Board is ok - I have tested it with LUFA demos.
The Truble is that MCU dont' interrupt when it recieved SETUP packet. Source should be UEINTX.RXSTPI, UEIENX.RXSTPE, , sei() enabled.
I made 'debugger' -output info on UART. What I see?
MCU caught USB General Interrupt as source bus reset and USB Endpoint Interrupt _only_ with UEINTX.TXINI.
I connected logic analiser - it showed that host sended DeviceDescriptor, but MCU didn't catch it.
I read datashet lot of times, + USB NutShell + particulary USB specification.
One more moment - I mean, MCU shoul recive 'body' DevDecsr request, but where It should be? UEBCLX always is 0.
I haven't any ideas.
"debugger" sends: R 08: 21 00 00: 00 18 00: 00 18 00: 00 18 00: 00 18 00: 00 18 00
R 08 - isn't wrong, you can find comented line.
R - reset, USB not initialized .
08 - reg. UEIENX before sei()
: 21 00 00 - UECONX and, copied from interrupt UDINT and UEINTX. UECONX.STALLRQ - Cleared by hardware when a new SETUP is received.(my small test)
: 00 18 00 - the same next times.
* - didn't print, ENDPOINT interrupt not called
Source code - bellow. Then - analiser report.
Code: Select all
LOG:
/*
* USB_sample.c
*
* Created: 20.01.2014 10:31:24
* Author: t.oleg
*/
#include <avr/io.h>
#include <avr/interrupt.h>
#include <avr/cpufunc.h>
#include <avr/wdt.h>
#include <util/delay.h>
#include <avr/power.h>
#include <avr/sleep.h>
#include <avr/pgmspace.h>
#define waitTXR while(!( UCSR1A & (1<<UDRE1))){;}
#define LED_ON PORTD &= ~(1<<4)
#define LED_OFF PORTD |= 1<<4
volatile uint8_t tmpreg1=0;
volatile uint8_t tmpreg2=0;
static inline void init_EP( const uint8_t EPN, const uint8_t UECFG0, const uint8_t UECFG1 );
static inline void conf_int_EP(const uint8_t EPN, const uint8_t INTMASK);
static void hexecho1 (uint8_t byte)
{
while (!( UCSR1A & (1<<UDRE1)))
{;}
UDR1 = ' ';
while (!( UCSR1A & (1<<UDRE1)))
{;}
if ((byte >> 4) < 0x0A)
{
UDR1 = (byte >> 4) + 0x30;
}
else
{
UDR1 = (byte >> 4) + 0x37;
}
while (!( UCSR1A & (1<<UDRE1)))
{;}
if ((byte & 0x0F) < 0x0A)
{
UDR1 = (byte & 0x0F) + 0x30;
}
else
{
UDR1 = (byte & 0x0F) + 0x37;
}
}
void USART_Init( const unsigned int baud )
{
/* Set baud rate*/
UBRR1H = (unsigned char)(baud>>8);
UBRR1L = (unsigned char)baud;
#define USE_2X 1
#if USE_2X
UCSR1A |= (1 << U2X1);
#else
UCSR1A &= ~(1 << U2X1);
#endif
/* Enable receiver and transmitter*/
UCSR1B = (1<<TXEN1); //|(1<<RXENn);
/* Set frame format: 8data, 2stop bit*/
// use reset values for 8N1 // UCSRnC = (1<<USBSn)|(3<<UCSZn0);
}
void setupHW(void)
{
/* Disable watchdog if enabled by bootloader/fuses */
MCUSR &= ~(1 << WDRF);
wdt_disable();
clock_prescale_set(clock_div_1); // так тактовая = частота кварца
DDRD |= 1<< 4;
DDRB |= 1<<PB7|1<<PB6|1<<PB5;
USART_Init( 8 );
}
void USBinit(void)
{
// USB_Init from LUFA
REGCR &= ~(1 << REGDIS); // disable Vreg
// USB_ResetInterface();
PLLCSR = ~(0<<PLLP0|0<<PLLP1|0<<PLLP2);
PLLCSR |= 1<<PLLE;
while (!(PLLCSR & (1<<PLOCK))); // wait PLL LOCK
USBCON = 0x20; //~(1 << USBE )|(1<<FRZCLK);
USBCON |= (1 << USBE);
USBCON &= ~(1<<FRZCLK);
init_EP(0, (uint8_t)~(1<<EPTYPE1|1<<EPTYPE0|1<<EPDIR), 0x00 ); // N0, control, 16 byte
//conf_int_EP(0, 1<<FLERRE|1<<NAKINE|1<<NAKOUTE|1<<RXSTPE|1<<RXOUTE|1<<STALLEDE|1<<TXINE);
conf_int_EP(0, 1<<RXSTPE);
// UEIENX = 1<<FLERRE|1<<NAKINE|1<<NAKOUTE|1<<RXSTPE|1<<RXOUTE|1<<STALLEDE|1<<TXINE; // all EP Interrupts for test
UDCON &= ~(1 << DETACH);
// Init USB by steps, p. 194
// Configure PLL interface
// Enable PLL
// Check PLL lock
// Enable USB interface
// Configure USB interface (USB Endpoint 0 configuration)
// Attach USB device
//UDIEN = 1<<UPRSME|1<<EORSME|1<<WAKEUPE|1<<EORSTE|1<<SOFE|1<<SUSPE; // use all interrupt for start
UDIEN = 1<<UPRSME|1<<EORSME|1<<EORSTE|1<<SOFE; // all, ex. WakeUP and SUSPEND
}
int main(void)
{
setupHW();
UDR1 = 'R';
USBinit();
hexecho1(UEIENX);
sei();
LED_OFF;
set_sleep_mode(SLEEP_MODE_IDLE);
sleep_enable();
while(1)
{
//TODO:: Please write your application code
waitTXR;
UDR1 = ':';
hexecho1(UECONX);
hexecho1(tmpreg1);
tmpreg1 = 0;
hexecho1(tmpreg2);
tmpreg2 = 0;
_NOP();
sleep_cpu();
LED_ON;
}
}
ISR(USB_GEN_vect, ISR_BLOCK)
{
static uint8_t cntGEN=0;
// Hardware Interface
cntGEN++;
tmpreg1 = UDINT;
if (UDINT & (1<<EORSTI)) {
// поймали сброс
UDINT &= ~(1<<EORSTI);
UERST |= 1 << 0|1<<1|1<<2|1<<3|1<<4; // reset EP 0
UDADDR = 0;
UDADDR |= 1 << ADDEN;
}
}
ISR(USB_COM_vect, ISR_BLOCK)
{
static uint8_t cntCOM=0;
// Endpoint events
cntCOM++;
tmpreg2 = UEINTX;
if (UEINTX & (1<<TXINI)) {
UEINTX &= ~(1<<TXINI);
}
sei();
waitTXR;
UDR1 = '*';
hexecho1(UECONX);
hexecho1(UESTA0X);
hexecho1(UESTA1X);
}
static void init_EP( const uint8_t EPN, const uint8_t UECFG0, const uint8_t UECFG1 )
{
// Endpoint initialization
// Endpoint activation, fig. 20-2
UENUM = EPN & 0x07; // last 3 bits
// UECONX |= 1<<STALLRQ;
UECONX |= 1<<EPEN|1<<STALLRQ;
UECFG0X = UECFG0 & 0xC3; // [7:6]EPTYPE, [0] EPDIR
UECFG1X = UECFG1 & 0x7E; // - [6:4]EPSIZE2:0, [3:2]EPBK1:0, [1] ALLOC
UECFG1X = 1<<ALLOC; // 16 bytes, one bank, do ALLOCATE
while (!(UESTA0X & (1<<CFGOK))); // wait ready
}
static void conf_int_EP(const uint8_t EPN, const uint8_t INTMASK)
{
// endpoint interrupt configure
UENUM = EPN;
UEIENX = INTMASK & ~(1<<5);
}
Code: Select all
Please wait...
USB RESET
11,31ms SOF 288
USB RESET
12,31ms SOF 289
13,31ms SOF 290
14,31ms SOF 291
15,31ms SOF 292
16,31ms SOF 293
17,31ms SOF 294
18,31ms SOF 295
19,31ms SOF 296
USB RESET
20,31ms SOF 297
21,31ms SOF 298
22,31ms SOF 299
23,31ms SOF 300
24,31ms SOF 301
25,31ms SOF 302
26,31ms SOF 303
27,31ms SOF 304
USB RESET
28,31ms SOF 305
29,31ms SOF 306
30,31ms SOF 307
31,31ms SOF 308
32,31ms SOF 309
33,31ms SOF 310
34,31ms SOF 311
35,31ms SOF 312
USB RESET
36,31ms SOF 313
37,31ms SOF 314
37,71ms SETUP Add: 0 EndPoint: 0 GET DESCRIPTOR DEVICE Length: 64 DATA0 80 06 00 01 00 00 40 00
37,73ms SETUP Add: 0 EndPoint: 0 GET DESCRIPTOR DEVICE Length: 64 DATA0 80 06 00 01 00 00 40 00
37,74ms SETUP Add: 0 EndPoint: 0 GET DESCRIPTOR DEVICE Length: 64 DATA0 80 06 00 01 00 00 40 00
38,31ms SOF 315
39,31ms SOF 316
40,31ms SOF 317
41,31ms SOF 318
42,31ms SOF 319
43,31ms SOF 320
USB RESET
44,31ms SOF 321
45,31ms SOF 322
46,31ms SOF 323
47,31ms SOF 324
48,31ms SOF 325
49,31ms SOF 326
50,31ms SOF 327
51,31ms SOF 328
No sync Found
51,32ms SOF 328
USB RESET
---.......-----
451,32ms SOF 728
USB RESET
452,32ms SOF 729
453,32ms SOF 730
454,32ms SOF 731
455,32ms SOF 732
456,32ms SOF 733
457,32ms SOF 734
458,32ms SOF 735
459,32ms SOF 736
USB RESET
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
463,32ms SOF 740
464,32ms SOF 741
465,32ms SOF 742
466,32ms SOF 743
467,32ms SOF 744
USB RESET
---.......---
539,32ms SOF 816
Invalid Token
No sync Found
Invalid Token
USB RESET
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
No sync Found
Invalid Token
542,32ms SOF 819
543,32ms SOF 820
544,32ms SOF 821
545,32ms SOF 822
546,32ms SOF 823
547,32ms SOF 824
USB RESET
548,32ms SOF 825
549,32ms SOF 826
550,32ms SOF 827
551,32ms SOF 828
552,32ms SOF 829
553,32ms SOF 830
USB RESET
565,32ms SOF 842
566,32ms SOF 843
567,32ms SOF 844
568,32ms SOF 845
569,32ms SOF 846
570,32ms SOF 847
571,32ms SOF 848
USB RESET
572,32ms SOF 849
573,32ms SOF 850
574,32ms SOF 851
575,32ms SOF 852
576,32ms SOF 853
577,32ms SOF 854
578,32ms SOF 855
579,32ms SOF 856
USB RESET
580,32ms SOF 857
581,32ms SOF 858
582,32ms SOF 859
583,32ms SOF 860
584,32ms SOF 861
585,32ms SOF 862
586,32ms SOF 863
587,32ms SOF 864
USB RESET
588,32ms SOF 865
589,32ms SOF 866
590,32ms SOF 867
591,32ms SOF 868
592,32ms SOF 869
593,32ms SOF 870
593,72ms SETUP Add: 0 EndPoint: 0 GET DESCRIPTOR DEVICE Length: 64 DATA0 80 06 00 01 00 00 40 00
593,74ms SETUP Add: 0 EndPoint: 0 GET DESCRIPTOR DEVICE Length: 64 DATA0 80 06 00 01 00 00 40 00
593,75ms SETUP Add: 0 EndPoint: 0 GET DESCRIPTOR DEVICE Length: 64 DATA0 80 06 00 01 00 00 40 00
594,32ms SOF 871
595,32ms SOF 872
USB RESET