- Fri Feb 15, 2013 4:40 am
#155623
I've decided to get round to sorting out my AVR programmer, which I've had for a while but never actually used since I got error messages in AVRDUDE. I'm getting the seemingly common "initialization failed, rc=-1 Double check connections and try again, or use -F to override this check" message. I've checked my connections god knows how many times and tried detecting both a Mega8 and Tiny2313 by typing "avrdude -c usbtiny -B 1 -pm8" and "avrdude -c usbtiny -B 1 -pt2313" respectively and neither of them work.
I am running 64-bit Windows 7, but as far as I can tell the drivers would appear to be working (I've swapped over the files from the libusb library and it shows up correctly under Device Manager). I'm supplying power through the AVR programmer and the 5V required is reaching the chips.
I am running 64-bit Windows 7, but as far as I can tell the drivers would appear to be working (I've swapped over the files from the libusb library and it shows up correctly under Device Manager). I'm supplying power through the AVR programmer and the 5V required is reaching the chips.