- Sat Jan 12, 2013 5:42 am
#154128
Hi, when I use stackable connectors on my shield ( the in-between shield) there are two point of concern, the contact area is less then a single row of pins (when non stackable shields are required). It seems to be close to a loose contact. The other point of concern is the open 2.5 mm gap between the shield and the Arduino UNO because the USB housing is restricting seating the board. I though of adding some isolated material between the shield and the connector, part of the Arduino UNO, to assure it's seated and possible some nylon screws/buses to make it 'industrial strength'. Any idea's what best practice is here? Reg. Piet