- Tue Oct 23, 2012 2:40 pm
#151009
Hello all,
I have a battery powered application using the Atemga 32u4 breakout that requires auto-detection of when USB power is connected, but not necessarily an actual USB connection (i.e. I need to know if I'm getting external power). From reading through the data sheet, I believe my code (pasted below) should be OK, and I think the issue may be in the setup of the USB hardware on the board (spark fun's atemga32u4 breakout).
It looks to me (though the Atmega data sheet is a bit vague here, but head to p253) that the pin connections of the breakout board are such that when USB power is disconnected, power to the entire USB module is killed, which disables the ability of the uC to monitor changes in the VBUS pin. The schematic for the breakout and the leonardo board differ here, in that it looks like the leonardo still powers the USB module even when VUSB is removed. From poking around it looks like the leonardo can detect a VBUS change (though I don't own one so can't verify), and I haven't seen anything online referring to VBUS monitoring with the atmega32u4 breakout or the pro micro.
When I use a multimeter to check the pin, I see a change of .8V (no usb) up to 5V(USB) on the VBUS/UVCC line, so the signal is there.
I know that I could add a switch or some other such thing, but I'm out of I/O pins and need to get this working without adding any additional interfacing. Also, this should be able to work, so I want to get it figured out since it's a useful application.
If anyone has any insight into the issue I'd greatly appreciate it. I think my next step is to try chopping the uVCC line to bring the atemga breakout into accordance with the leonardo and the data sheet.
-Shibbs
Here's my code below :
Sparkfun's breakout schematic : http://dlnmh9ip6v2uc.cloudfront.net/dat ... ut-v11.pdf
leonardo schematic : http://www.amr-geneve.ch/wp-content/upl ... tic_3b.pdf
atmega datasheet : http://www.atmel.com/Images/doc7766.pdf
I have a battery powered application using the Atemga 32u4 breakout that requires auto-detection of when USB power is connected, but not necessarily an actual USB connection (i.e. I need to know if I'm getting external power). From reading through the data sheet, I believe my code (pasted below) should be OK, and I think the issue may be in the setup of the USB hardware on the board (spark fun's atemga32u4 breakout).
It looks to me (though the Atmega data sheet is a bit vague here, but head to p253) that the pin connections of the breakout board are such that when USB power is disconnected, power to the entire USB module is killed, which disables the ability of the uC to monitor changes in the VBUS pin. The schematic for the breakout and the leonardo board differ here, in that it looks like the leonardo still powers the USB module even when VUSB is removed. From poking around it looks like the leonardo can detect a VBUS change (though I don't own one so can't verify), and I haven't seen anything online referring to VBUS monitoring with the atmega32u4 breakout or the pro micro.
When I use a multimeter to check the pin, I see a change of .8V (no usb) up to 5V(USB) on the VBUS/UVCC line, so the signal is there.
I know that I could add a switch or some other such thing, but I'm out of I/O pins and need to get this working without adding any additional interfacing. Also, this should be able to work, so I want to get it figured out since it's a useful application.
If anyone has any insight into the issue I'd greatly appreciate it. I think my next step is to try chopping the uVCC line to bring the atemga breakout into accordance with the leonardo and the data sheet.
-Shibbs
Here's my code below :
Code: Select all
Here are the schematics for the boards in question : //code is compiled and loaded with the Aduion 1.1IDE under the Leonardo boot loader
void setup(){
//macros to turn on board power and set up the LEDs
POWER_ON;
R_LED_INIT_OUTPUT;
G_LED1_INIT_OUTPUT;
G_LED1_OFF;
G_LED2_INIT_OUTPUT;
G_LED2_OFF;
delay(3000);
//USB init
USBCON |= (1<<USBE)|(1<<VBUSTE)|(1<< OTGPADE) ; //enable the Vbus transition enable, as well as enable the USB module
UHWCON |= 1<<UVREGE; //turns on the internal regulator, shouldn't be necessaary, but was added later as a check
sei(); //enable interrupts
}
void loop(){
//breathe the red LED every 2 seconds
POWER_ON;
R_LED_ON;
delay(2000);
R_LED_OFF;
delay(2000);
//checks the USB power registers
if( (USBSTA | (1<<VBUS)) ==0 ) // check the value of the VBUS pin
G_LED1_ON;
else G_LED1_OFF; //this is the line that gets executed, indicating VBUS is always found ot be low
if( ( USBINT|(1<<VBUSTI)) !=0){ //check the VBus transition interrupt
B_LED_ON; //this is evaluated as true always
}else B_LED_OFF;
USBINT &= ~(1<<VBUSTI); //clear the flag
}
//as best as I cna tell, neither interrupt is ever entere into
ISR(USB_GENERAL_vect){
//Serial.println("saw a change");
G_LED1_ON;
USBINT &= ~(1<<VBUSTI);
}
ISR(USB_ENDPOINT_vect){
//Serial.println("saw a change");
G_LED1_ON;
USBINT &= ~(1<<VBUSTI);
}
Sparkfun's breakout schematic : http://dlnmh9ip6v2uc.cloudfront.net/dat ... ut-v11.pdf
leonardo schematic : http://www.amr-geneve.ch/wp-content/upl ... tic_3b.pdf
atmega datasheet : http://www.atmel.com/Images/doc7766.pdf