- Sun Jul 31, 2011 3:02 pm
#131066
First off, here is my environment:
Gentoo Linux (kernel 2.6.36-gentoo-r5)
avr-gcc 4.5.2
avrdude 5.5
Updated avrdude.conf for atmega328p
Atmega328p microcontroller
So I went through the sparkfun tutorial, connected everything.
I then went and compiled blink_1MHz.c (successfully).
Then I ran avrdude (after configuration) using
Any help would be appreciated.
Thanks,
Chuck
Gentoo Linux (kernel 2.6.36-gentoo-r5)
avr-gcc 4.5.2
avrdude 5.5
Updated avrdude.conf for atmega328p
Atmega328p microcontroller
So I went through the sparkfun tutorial, connected everything.
I then went and compiled blink_1MHz.c (successfully).
Then I ran avrdude (after configuration) using
# make programand it looks like avrdude completes successfully
avrdude -p atmega328p -P /dev/parport0 -c stk200 -v -v -U flash:w:blink_1MHz.hexProblem is that the LED still doesn't blink. I tested the LEDs and they all seem to work independently of the controller.
avrdude: Version 5.5, compiled on Mar 5 2011 at 19:58:36
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
System wide configuration file is "/etc/avrdude.conf"
User configuration file is "/home/cwinters/.avrduderc"
User configuration file does not exist or is not a regular file, skipping
Using Port : /dev/parport0
Using Programmer : stk200
AVR Part : ATMEGA328P
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PC2
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
eeprom 65 5 4 0 no 1024 4 0 3600 3600 0xff 0xff
flash 65 6 128 0 yes 32768 128 256 4500 4500 0xff 0xff
lfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
efuse 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
lock 0 0 0 0 no 1 0 0 4500 4500 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
Programmer Type : PPI
Description : STK200
VCC = (not used)
BUFF = 4,5
RESET = 9
SCK = 6
MOSI = 7
MISO = 10
ERR LED = 0
RDY LED = 0
PGM LED = 0
VFY LED = 0
avrdude: Calibrating delay loop... calibrated to 499 cycles per us
bitbang_cmd(): [ AC 53 00 00 ] [ FF FF 53 00 ]
avrdude: AVR device initialized and ready to accept instructions
Reading | bitbang_cmd(): [ 30 00 00 00 ] [ 00 30 00 1E ]
bitbang_cmd(): [ 30 00 01 00 ] [ 00 30 00 95 ]
################bitbang_cmd(): [ 30 00 02 00 ] [ 00 30 00 0F ]
################################## | 100% 0.00s
avrdude: Device signature = 0x1e950f
bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]
bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]
bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]
avrdude: safemode: lfuse reads as 62
bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]
bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]
bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]
avrdude: safemode: hfuse reads as D9
bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]
bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]
bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]
avrdude: safemode: efuse reads as 7
avrdude: NOTE: FLASH memory has been specified, an erase cycle will be performed
To disable this feature, specify the -D option.
bitbang_cmd(): [ A0 03 FC 00 ] [ 00 A0 03 FF ]
bitbang_cmd(): [ A0 03 FD 00 ] [ 00 A0 03 FF ]
bitbang_cmd(): [ A0 03 FE 00 ] [ 00 A0 03 FF ]
bitbang_cmd(): [ A0 03 FF 00 ] [ 00 A0 03 FF ]
avrdude: erasing chip
bitbang_cmd(): [ AC 80 00 00 ] [ 00 AC 80 00 ]
avrdude: Calibrating delay loop... calibrated to 497 cycles per us
bitbang_cmd(): [ AC 53 00 00 ] [ FF FF 53 00 ]
avrdude: reading input file "blink_1MHz.hex"
avrdude: input file blink_1MHz.hex auto detected as Intel Hex
avrdude: writing flash (248 bytes):
Writing | bitbang_cmd(): [ 40 00 00 0C ] [ 00 40 00 00 ]
bitbang_cmd(): [ 48 00 00 94 ] [ 0C 48 00 00 ]
bitbang_cmd(): [ 40 00 01 34 ] [ 94 40 00 01 ]
bitbang_cmd(): [ 48 00 01 00 ] [ 34 48 00 01 ]
bitbang_cmd(): [ 40 00 02 0C ] [ 00 40 00 02 ]
#bitbang_cmd(): [ 48 00 02 94 ] [ 0C 48 00 02 ]
bitbang_cmd(): [ 40 00 03 51 ] [ 94 40 00 03 ]
bitbang_cmd(): [ 48 00 03 00 ] [ 51 48 00 03 ]
bitbang_cmd(): [ 40 00 04 0C ] [ 00 40 00 04 ]
bitbang_cmd(): [ 48 00 04 94 ] [ 0C 48 00 04 ]
#bitbang_cmd(): [ 40 00 05 51 ] [ 94 40 00 05 ]
bitbang_cmd(): [ 48 00 05 00 ] [ 51 48 00 05 ]
bitbang_cmd(): [ 40 00 06 0C ] [ 00 40 00 06 ]
bitbang_cmd(): [ 48 00 06 94 ] [ 0C 48 00 06 ]
bitbang_cmd(): [ 40 00 07 51 ] [ 94 40 00 07 ]
#bitbang_cmd(): [ 48 00 07 00 ] [ 51 48 00 07 ]
bitbang_cmd(): [ 40 00 08 0C ] [ 00 40 00 08 ]
bitbang_cmd(): [ 48 00 08 94 ] [ 0C 48 00 08 ]
bitbang_cmd(): [ 40 00 09 51 ] [ 94 40 00 09 ]
bitbang_cmd(): [ 48 00 09 00 ] [ 51 48 00 09 ]
#bitbang_cmd(): [ 40 00 0A 0C ] [ 00 40 00 0A ]
bitbang_cmd(): [ 48 00 0A 94 ] [ 0C 48 00 0A ]
bitbang_cmd(): [ 40 00 0B 51 ] [ 94 40 00 0B ]
bitbang_cmd(): [ 48 00 0B 00 ] [ 51 48 00 0B ]
bitbang_cmd(): [ 40 00 0C 0C ] [ 00 40 00 0C ]
#bitbang_cmd(): [ 48 00 0C 94 ] [ 0C 48 00 0C ]
bitbang_cmd(): [ 40 00 0D 51 ] [ 94 40 00 0D ]
bitbang_cmd(): [ 48 00 0D 00 ] [ 51 48 00 0D ]
bitbang_cmd(): [ 40 00 0E 0C ] [ 00 40 00 0E ]
bitbang_cmd(): [ 48 00 0E 94 ] [ 0C 48 00 0E ]
#bitbang_cmd(): [ 40 00 0F 51 ] [ 94 40 00 0F ]
bitbang_cmd(): [ 48 00 0F 00 ] [ 51 48 00 0F ]
bitbang_cmd(): [ 40 00 10 0C ] [ 00 40 00 10 ]
bitbang_cmd(): [ 48 00 10 94 ] [ 0C 48 00 10 ]
bitbang_cmd(): [ 40 00 11 51 ] [ 94 40 00 11 ]
#bitbang_cmd(): [ 48 00 11 00 ] [ 51 48 00 11 ]
bitbang_cmd(): [ 40 00 12 0C ] [ 00 40 00 12 ]
bitbang_cmd(): [ 48 00 12 94 ] [ 0C 48 00 12 ]
bitbang_cmd(): [ 40 00 13 51 ] [ 94 40 00 13 ]
bitbang_cmd(): [ 48 00 13 00 ] [ 51 48 00 13 ]
#bitbang_cmd(): [ 40 00 14 0C ] [ 00 40 00 14 ]
bitbang_cmd(): [ 48 00 14 94 ] [ 0C 48 00 14 ]
bitbang_cmd(): [ 40 00 15 51 ] [ 94 40 00 15 ]
bitbang_cmd(): [ 48 00 15 00 ] [ 51 48 00 15 ]
bitbang_cmd(): [ 40 00 16 0C ] [ 00 40 00 16 ]
#bitbang_cmd(): [ 48 00 16 94 ] [ 0C 48 00 16 ]
bitbang_cmd(): [ 40 00 17 51 ] [ 94 40 00 17 ]
bitbang_cmd(): [ 48 00 17 00 ] [ 51 48 00 17 ]
bitbang_cmd(): [ 40 00 18 0C ] [ 00 40 00 18 ]
bitbang_cmd(): [ 48 00 18 94 ] [ 0C 48 00 18 ]
#bitbang_cmd(): [ 40 00 19 51 ] [ 94 40 00 19 ]
bitbang_cmd(): [ 48 00 19 00 ] [ 51 48 00 19 ]
bitbang_cmd(): [ 40 00 1A 0C ] [ 00 40 00 1A ]
bitbang_cmd(): [ 48 00 1A 94 ] [ 0C 48 00 1A ]
bitbang_cmd(): [ 40 00 1B 51 ] [ 94 40 00 1B ]
#bitbang_cmd(): [ 48 00 1B 00 ] [ 51 48 00 1B ]
bitbang_cmd(): [ 40 00 1C 0C ] [ 00 40 00 1C ]
bitbang_cmd(): [ 48 00 1C 94 ] [ 0C 48 00 1C ]
bitbang_cmd(): [ 40 00 1D 51 ] [ 94 40 00 1D ]
bitbang_cmd(): [ 48 00 1D 00 ] [ 51 48 00 1D ]
#bitbang_cmd(): [ 40 00 1E 0C ] [ 00 40 00 1E ]
bitbang_cmd(): [ 48 00 1E 94 ] [ 0C 48 00 1E ]
bitbang_cmd(): [ 40 00 1F 51 ] [ 94 40 00 1F ]
bitbang_cmd(): [ 48 00 1F 00 ] [ 51 48 00 1F ]
bitbang_cmd(): [ 40 00 20 0C ] [ 00 40 00 20 ]
#bitbang_cmd(): [ 48 00 20 94 ] [ 0C 48 00 20 ]
bitbang_cmd(): [ 40 00 21 51 ] [ 94 40 00 21 ]
bitbang_cmd(): [ 48 00 21 00 ] [ 51 48 00 21 ]
bitbang_cmd(): [ 40 00 22 0C ] [ 00 40 00 22 ]
bitbang_cmd(): [ 48 00 22 94 ] [ 0C 48 00 22 ]
#bitbang_cmd(): [ 40 00 23 51 ] [ 94 40 00 23 ]
bitbang_cmd(): [ 48 00 23 00 ] [ 51 48 00 23 ]
bitbang_cmd(): [ 40 00 24 0C ] [ 00 40 00 24 ]
bitbang_cmd(): [ 48 00 24 94 ] [ 0C 48 00 24 ]
bitbang_cmd(): [ 40 00 25 51 ] [ 94 40 00 25 ]
#bitbang_cmd(): [ 48 00 25 00 ] [ 51 48 00 25 ]
bitbang_cmd(): [ 40 00 26 0C ] [ 00 40 00 26 ]
bitbang_cmd(): [ 48 00 26 94 ] [ 0C 48 00 26 ]
bitbang_cmd(): [ 40 00 27 51 ] [ 94 40 00 27 ]
bitbang_cmd(): [ 48 00 27 00 ] [ 51 48 00 27 ]
#bitbang_cmd(): [ 40 00 28 0C ] [ 00 40 00 28 ]
bitbang_cmd(): [ 48 00 28 94 ] [ 0C 48 00 28 ]
bitbang_cmd(): [ 40 00 29 51 ] [ 94 40 00 29 ]
bitbang_cmd(): [ 48 00 29 00 ] [ 51 48 00 29 ]
bitbang_cmd(): [ 40 00 2A 0C ] [ 00 40 00 2A ]
#bitbang_cmd(): [ 48 00 2A 94 ] [ 0C 48 00 2A ]
bitbang_cmd(): [ 40 00 2B 51 ] [ 94 40 00 2B ]
bitbang_cmd(): [ 48 00 2B 00 ] [ 51 48 00 2B ]
bitbang_cmd(): [ 40 00 2C 0C ] [ 00 40 00 2C ]
bitbang_cmd(): [ 48 00 2C 94 ] [ 0C 48 00 2C ]
#bitbang_cmd(): [ 40 00 2D 51 ] [ 94 40 00 2D ]
bitbang_cmd(): [ 48 00 2D 00 ] [ 51 48 00 2D ]
bitbang_cmd(): [ 40 00 2E 0C ] [ 00 40 00 2E ]
bitbang_cmd(): [ 48 00 2E 94 ] [ 0C 48 00 2E ]
bitbang_cmd(): [ 40 00 2F 51 ] [ 94 40 00 2F ]
#bitbang_cmd(): [ 48 00 2F 00 ] [ 51 48 00 2F ]
bitbang_cmd(): [ 40 00 30 0C ] [ 00 40 00 30 ]
bitbang_cmd(): [ 48 00 30 94 ] [ 0C 48 00 30 ]
bitbang_cmd(): [ 40 00 31 51 ] [ 94 40 00 31 ]
bitbang_cmd(): [ 48 00 31 00 ] [ 51 48 00 31 ]
#bitbang_cmd(): [ 40 00 32 0C ] [ 00 40 00 32 ]
bitbang_cmd(): [ 48 00 32 94 ] [ 0C 48 00 32 ]
bitbang_cmd(): [ 40 00 33 51 ] [ 94 40 00 33 ]
bitbang_cmd(): [ 48 00 33 00 ] [ 51 48 00 33 ]
bitbang_cmd(): [ 40 00 34 11 ] [ 00 40 00 34 ]
#bitbang_cmd(): [ 48 00 34 24 ] [ 11 48 00 34 ]
bitbang_cmd(): [ 40 00 35 1F ] [ 24 40 00 35 ]
bitbang_cmd(): [ 48 00 35 BE ] [ 1F 48 00 35 ]
bitbang_cmd(): [ 40 00 36 CF ] [ BE 40 00 36 ]
bitbang_cmd(): [ 48 00 36 EF ] [ CF 48 00 36 ]
#bitbang_cmd(): [ 40 00 37 D8 ] [ EF 40 00 37 ]
bitbang_cmd(): [ 48 00 37 E0 ] [ D8 48 00 37 ]
bitbang_cmd(): [ 40 00 38 DE ] [ E0 40 00 38 ]
bitbang_cmd(): [ 48 00 38 BF ] [ DE 48 00 38 ]
bitbang_cmd(): [ 40 00 39 CD ] [ BF 40 00 39 ]
#bitbang_cmd(): [ 48 00 39 BF ] [ CD 48 00 39 ]
bitbang_cmd(): [ 40 00 3A 11 ] [ BF 40 00 3A ]
bitbang_cmd(): [ 48 00 3A E0 ] [ 11 48 00 3A ]
bitbang_cmd(): [ 40 00 3B A0 ] [ E0 40 00 3B ]
bitbang_cmd(): [ 48 00 3B E0 ] [ A0 48 00 3B ]
#bitbang_cmd(): [ 40 00 3C B1 ] [ E0 40 00 3C ]
bitbang_cmd(): [ 48 00 3C E0 ] [ B1 48 00 3C ]
bitbang_cmd(): [ 40 00 3D E8 ] [ E0 40 00 3D ]
bitbang_cmd(): [ 48 00 3D EF ] [ E8 48 00 3D ]
#bitbang_cmd(): [ 40 00 3E F0 ] [ EF 40 00 3E ]
bitbang_cmd(): [ 48 00 3E E0 ] [ F0 48 00 3E ]
bitbang_cmd(): [ 40 00 3F 02 ] [ E0 40 00 3F ]
bitbang_cmd(): [ 48 00 3F C0 ] [ 02 48 00 3F ]
bitbang_cmd(): [ 4C 00 00 00 ] [ C0 4C 00 00 ]
bitbang_cmd(): [ 40 00 00 05 ] [ 00 40 00 00 ]
#bitbang_cmd(): [ 48 00 00 90 ] [ 05 48 00 00 ]
bitbang_cmd(): [ 40 00 01 0D ] [ 90 40 00 01 ]
bitbang_cmd(): [ 48 00 01 92 ] [ 0D 48 00 01 ]
bitbang_cmd(): [ 40 00 02 A0 ] [ 92 40 00 02 ]
bitbang_cmd(): [ 48 00 02 30 ] [ A0 48 00 02 ]
#bitbang_cmd(): [ 40 00 03 B1 ] [ 30 40 00 03 ]
bitbang_cmd(): [ 48 00 03 07 ] [ B1 48 00 03 ]
bitbang_cmd(): [ 40 00 04 D9 ] [ 07 40 00 04 ]
bitbang_cmd(): [ 48 00 04 F7 ] [ D9 48 00 04 ]
bitbang_cmd(): [ 40 00 05 11 ] [ F7 40 00 05 ]
#bitbang_cmd(): [ 48 00 05 E0 ] [ 11 48 00 05 ]
bitbang_cmd(): [ 40 00 06 A0 ] [ E0 40 00 06 ]
bitbang_cmd(): [ 48 00 06 E0 ] [ A0 48 00 06 ]
bitbang_cmd(): [ 40 00 07 B1 ] [ E0 40 00 07 ]
bitbang_cmd(): [ 48 00 07 E0 ] [ B1 48 00 07 ]
#bitbang_cmd(): [ 40 00 08 01 ] [ E0 40 00 08 ]
bitbang_cmd(): [ 48 00 08 C0 ] [ 01 48 00 08 ]
bitbang_cmd(): [ 40 00 09 1D ] [ C0 40 00 09 ]
bitbang_cmd(): [ 48 00 09 92 ] [ 1D 48 00 09 ]
bitbang_cmd(): [ 40 00 0A A0 ] [ 92 40 00 0A ]
#bitbang_cmd(): [ 48 00 0A 30 ] [ A0 48 00 0A ]
bitbang_cmd(): [ 40 00 0B B1 ] [ 30 40 00 0B ]
bitbang_cmd(): [ 48 00 0B 07 ] [ B1 48 00 0B ]
bitbang_cmd(): [ 40 00 0C E1 ] [ 07 40 00 0C ]
bitbang_cmd(): [ 48 00 0C F7 ] [ E1 48 00 0C ]
#bitbang_cmd(): [ 40 00 0D 0E ] [ F7 40 00 0D ]
bitbang_cmd(): [ 48 00 0D 94 ] [ 0E 48 00 0D ]
bitbang_cmd(): [ 40 00 0E 67 ] [ 94 40 00 0E ]
bitbang_cmd(): [ 48 00 0E 00 ] [ 67 48 00 0E ]
bitbang_cmd(): [ 40 00 0F 0C ] [ 00 40 00 0F ]
#bitbang_cmd(): [ 48 00 0F 94 ] [ 0C 48 00 0F ]
bitbang_cmd(): [ 40 00 10 7A ] [ 94 40 00 10 ]
bitbang_cmd(): [ 48 00 10 00 ] [ 7A 48 00 10 ]
bitbang_cmd(): [ 40 00 11 0C ] [ 00 40 00 11 ]
bitbang_cmd(): [ 48 00 11 94 ] [ 0C 48 00 11 ]
#bitbang_cmd(): [ 40 00 12 00 ] [ 94 40 00 12 ]
bitbang_cmd(): [ 48 00 12 00 ] [ 00 48 00 12 ]
bitbang_cmd(): [ 40 00 13 8F ] [ 00 40 00 13 ]
bitbang_cmd(): [ 48 00 13 EF ] [ 8F 48 00 13 ]
bitbang_cmd(): [ 40 00 14 84 ] [ EF 40 00 14 ]
#bitbang_cmd(): [ 48 00 14 B9 ] [ 84 48 00 14 ]
bitbang_cmd(): [ 40 00 15 87 ] [ B9 40 00 15 ]
bitbang_cmd(): [ 48 00 15 B9 ] [ 87 48 00 15 ]
bitbang_cmd(): [ 40 00 16 8E ] [ B9 40 00 16 ]
bitbang_cmd(): [ 48 00 16 EF ] [ 8E 48 00 16 ]
#bitbang_cmd(): [ 40 00 17 8A ] [ EF 40 00 17 ]
bitbang_cmd(): [ 48 00 17 B9 ] [ 8A 48 00 17 ]
bitbang_cmd(): [ 40 00 18 08 ] [ B9 40 00 18 ]
bitbang_cmd(): [ 48 00 18 95 ] [ 08 48 00 18 ]
bitbang_cmd(): [ 40 00 19 0A ] [ 95 40 00 19 ]
#bitbang_cmd(): [ 48 00 19 C0 ] [ 0A 48 00 19 ]
bitbang_cmd(): [ 40 00 1A 2A ] [ C0 40 00 1A ]
bitbang_cmd(): [ 48 00 1A E5 ] [ 2A 48 00 1A ]
bitbang_cmd(): [ 40 00 1B 00 ] [ E5 40 00 1B ]
bitbang_cmd(): [ 48 00 1B 00 ] [ 00 48 00 1B ]
#bitbang_cmd(): [ 40 00 1C 00 ] [ 00 40 00 1C ]
bitbang_cmd(): [ 48 00 1C 00 ] [ 00 48 00 1C ]
bitbang_cmd(): [ 40 00 1D 00 ] [ 00 40 00 1D ]
bitbang_cmd(): [ 48 00 1D 00 ] [ 00 48 00 1D ]
bitbang_cmd(): [ 40 00 1E 00 ] [ 00 40 00 1E ]
#bitbang_cmd(): [ 48 00 1E 00 ] [ 00 48 00 1E ]
bitbang_cmd(): [ 40 00 1F 00 ] [ 00 40 00 1F ]
bitbang_cmd(): [ 48 00 1F 00 ] [ 00 48 00 1F ]
bitbang_cmd(): [ 40 00 20 00 ] [ 00 40 00 20 ]
bitbang_cmd(): [ 48 00 20 00 ] [ 00 48 00 20 ]
#bitbang_cmd(): [ 40 00 21 21 ] [ 00 40 00 21 ]
bitbang_cmd(): [ 48 00 21 50 ] [ 21 48 00 21 ]
bitbang_cmd(): [ 40 00 22 C1 ] [ 50 40 00 22 ]
bitbang_cmd(): [ 48 00 22 F7 ] [ C1 48 00 22 ]
bitbang_cmd(): [ 40 00 23 01 ] [ F7 40 00 23 ]
#bitbang_cmd(): [ 48 00 23 97 ] [ 01 48 00 23 ]
bitbang_cmd(): [ 40 00 24 00 ] [ 97 40 00 24 ]
bitbang_cmd(): [ 48 00 24 97 ] [ 00 48 00 24 ]
bitbang_cmd(): [ 40 00 25 A1 ] [ 97 40 00 25 ]
bitbang_cmd(): [ 48 00 25 F7 ] [ A1 48 00 25 ]
#bitbang_cmd(): [ 40 00 26 08 ] [ F7 40 00 26 ]
bitbang_cmd(): [ 48 00 26 95 ] [ 08 48 00 26 ]
bitbang_cmd(): [ 40 00 27 1F ] [ 95 40 00 27 ]
bitbang_cmd(): [ 48 00 27 93 ] [ 1F 48 00 27 ]
bitbang_cmd(): [ 40 00 28 0E ] [ 93 40 00 28 ]
#bitbang_cmd(): [ 48 00 28 94 ] [ 0E 48 00 28 ]
bitbang_cmd(): [ 40 00 29 53 ] [ 94 40 00 29 ]
bitbang_cmd(): [ 48 00 29 00 ] [ 53 48 00 29 ]
bitbang_cmd(): [ 40 00 2A 1F ] [ 00 40 00 2A ]
bitbang_cmd(): [ 48 00 2A EF ] [ 1F 48 00 2A ]
#bitbang_cmd(): [ 40 00 2B 18 ] [ EF 40 00 2B ]
bitbang_cmd(): [ 48 00 2B B9 ] [ 18 48 00 2B ]
bitbang_cmd(): [ 40 00 2C 15 ] [ B9 40 00 2C ]
bitbang_cmd(): [ 48 00 2C B9 ] [ 15 48 00 2C ]
bitbang_cmd(): [ 40 00 2D 1B ] [ B9 40 00 2D ]
#bitbang_cmd(): [ 48 00 2D B9 ] [ 1B 48 00 2D ]
bitbang_cmd(): [ 40 00 2E 84 ] [ B9 40 00 2E ]
bitbang_cmd(): [ 48 00 2E EF ] [ 84 48 00 2E ]
bitbang_cmd(): [ 40 00 2F 91 ] [ EF 40 00 2F ]
bitbang_cmd(): [ 48 00 2F E0 ] [ 91 48 00 2F ]
#bitbang_cmd(): [ 40 00 30 0E ] [ E0 40 00 30 ]
bitbang_cmd(): [ 48 00 30 94 ] [ 0E 48 00 30 ]
bitbang_cmd(): [ 40 00 31 59 ] [ 94 40 00 31 ]
bitbang_cmd(): [ 48 00 31 00 ] [ 59 48 00 31 ]
bitbang_cmd(): [ 40 00 32 18 ] [ 00 40 00 32 ]
#bitbang_cmd(): [ 48 00 32 B8 ] [ 18 48 00 32 ]
bitbang_cmd(): [ 40 00 33 15 ] [ B8 40 00 33 ]
bitbang_cmd(): [ 48 00 33 B8 ] [ 15 48 00 33 ]
bitbang_cmd(): [ 40 00 34 1B ] [ B8 40 00 34 ]
bitbang_cmd(): [ 48 00 34 B8 ] [ 1B 48 00 34 ]
#bitbang_cmd(): [ 40 00 35 84 ] [ B8 40 00 35 ]
bitbang_cmd(): [ 48 00 35 EF ] [ 84 48 00 35 ]
bitbang_cmd(): [ 40 00 36 91 ] [ EF 40 00 36 ]
bitbang_cmd(): [ 48 00 36 E0 ] [ 91 48 00 36 ]
bitbang_cmd(): [ 40 00 37 0E ] [ E0 40 00 37 ]
#bitbang_cmd(): [ 48 00 37 94 ] [ 0E 48 00 37 ]
bitbang_cmd(): [ 40 00 38 59 ] [ 94 40 00 38 ]
bitbang_cmd(): [ 48 00 38 00 ] [ 59 48 00 38 ]
bitbang_cmd(): [ 40 00 39 F1 ] [ 00 40 00 39 ]
bitbang_cmd(): [ 48 00 39 CF ] [ F1 48 00 39 ]
#bitbang_cmd(): [ 40 00 3A F8 ] [ CF 40 00 3A ]
bitbang_cmd(): [ 48 00 3A 94 ] [ F8 48 00 3A ]
bitbang_cmd(): [ 40 00 3B FF ] [ 94 40 00 3B ]
bitbang_cmd(): [ 48 00 3B CF ] [ FF 48 00 3B ]
bitbang_cmd(): [ 4C 00 40 00 ] [ CF 4C 00 40 ]
# | 100% 0.10s
avrdude: 248 bytes of flash written
avrdude: verifying flash memory against blink_1MHz.hex:
avrdude: load data flash data from input file blink_1MHz.hex:
avrdude: input file blink_1MHz.hex auto detected as Intel Hex
avrdude: input file blink_1MHz.hex contains 248 bytes
avrdude: reading on-chip flash data:
Reading | bitbang_cmd(): [ 20 00 00 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 00 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 01 00 ] [ 00 20 00 34 ]
bitbang_cmd(): [ 28 00 01 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 02 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 02 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 03 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 03 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 04 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 04 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 05 00 ] [ 00 20 00 51 ]
#bitbang_cmd(): [ 28 00 05 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 06 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 06 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 07 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 07 00 ] [ 00 28 00 00 ]
#bitbang_cmd(): [ 20 00 08 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 08 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 09 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 09 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 0A 00 ] [ 00 20 00 0C ]
#bitbang_cmd(): [ 28 00 0A 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 0B 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 0B 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 0C 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 0C 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 0D 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 0D 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 0E 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 0E 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 0F 00 ] [ 00 20 00 51 ]
#bitbang_cmd(): [ 28 00 0F 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 10 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 10 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 11 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 11 00 ] [ 00 28 00 00 ]
#bitbang_cmd(): [ 20 00 12 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 12 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 13 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 13 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 14 00 ] [ 00 20 00 0C ]
#bitbang_cmd(): [ 28 00 14 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 15 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 15 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 16 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 16 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 17 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 17 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 18 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 18 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 19 00 ] [ 00 20 00 51 ]
#bitbang_cmd(): [ 28 00 19 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 1A 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 1A 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 1B 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 1B 00 ] [ 00 28 00 00 ]
#bitbang_cmd(): [ 20 00 1C 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 1C 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 1D 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 1D 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 1E 00 ] [ 00 20 00 0C ]
#bitbang_cmd(): [ 28 00 1E 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 1F 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 1F 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 20 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 20 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 21 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 21 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 22 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 22 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 23 00 ] [ 00 20 00 51 ]
#bitbang_cmd(): [ 28 00 23 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 24 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 24 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 25 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 25 00 ] [ 00 28 00 00 ]
#bitbang_cmd(): [ 20 00 26 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 26 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 27 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 27 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 28 00 ] [ 00 20 00 0C ]
#bitbang_cmd(): [ 28 00 28 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 29 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 29 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 2A 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 2A 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 2B 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 2B 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 2C 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 2C 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 2D 00 ] [ 00 20 00 51 ]
#bitbang_cmd(): [ 28 00 2D 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 2E 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 2E 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 2F 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 2F 00 ] [ 00 28 00 00 ]
#bitbang_cmd(): [ 20 00 30 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 30 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 31 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 31 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 32 00 ] [ 00 20 00 0C ]
#bitbang_cmd(): [ 28 00 32 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 33 00 ] [ 00 20 00 51 ]
bitbang_cmd(): [ 28 00 33 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 34 00 ] [ 00 20 00 11 ]
bitbang_cmd(): [ 28 00 34 00 ] [ 00 28 00 24 ]
#bitbang_cmd(): [ 20 00 35 00 ] [ 00 20 00 1F ]
bitbang_cmd(): [ 28 00 35 00 ] [ 00 28 00 BE ]
bitbang_cmd(): [ 20 00 36 00 ] [ 00 20 00 CF ]
bitbang_cmd(): [ 28 00 36 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 37 00 ] [ 00 20 00 D8 ]
#bitbang_cmd(): [ 28 00 37 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 38 00 ] [ 00 20 00 DE ]
bitbang_cmd(): [ 28 00 38 00 ] [ 00 28 00 BF ]
bitbang_cmd(): [ 20 00 39 00 ] [ 00 20 00 CD ]
bitbang_cmd(): [ 28 00 39 00 ] [ 00 28 00 BF ]
#bitbang_cmd(): [ 20 00 3A 00 ] [ 00 20 00 11 ]
bitbang_cmd(): [ 28 00 3A 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 3B 00 ] [ 00 20 00 A0 ]
bitbang_cmd(): [ 28 00 3B 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 3C 00 ] [ 00 20 00 B1 ]
#bitbang_cmd(): [ 28 00 3C 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 3D 00 ] [ 00 20 00 E8 ]
bitbang_cmd(): [ 28 00 3D 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 3E 00 ] [ 00 20 00 F0 ]
#bitbang_cmd(): [ 28 00 3E 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 3F 00 ] [ 00 20 00 02 ]
bitbang_cmd(): [ 28 00 3F 00 ] [ 00 28 00 C0 ]
bitbang_cmd(): [ 20 00 40 00 ] [ 00 20 00 05 ]
bitbang_cmd(): [ 28 00 40 00 ] [ 00 28 00 90 ]
#bitbang_cmd(): [ 20 00 41 00 ] [ 00 20 00 0D ]
bitbang_cmd(): [ 28 00 41 00 ] [ 00 28 00 92 ]
bitbang_cmd(): [ 20 00 42 00 ] [ 00 20 00 A0 ]
bitbang_cmd(): [ 28 00 42 00 ] [ 00 28 00 30 ]
bitbang_cmd(): [ 20 00 43 00 ] [ 00 20 00 B1 ]
#bitbang_cmd(): [ 28 00 43 00 ] [ 00 28 00 07 ]
bitbang_cmd(): [ 20 00 44 00 ] [ 00 20 00 D9 ]
bitbang_cmd(): [ 28 00 44 00 ] [ 00 28 00 F7 ]
bitbang_cmd(): [ 20 00 45 00 ] [ 00 20 00 11 ]
bitbang_cmd(): [ 28 00 45 00 ] [ 00 28 00 E0 ]
#bitbang_cmd(): [ 20 00 46 00 ] [ 00 20 00 A0 ]
bitbang_cmd(): [ 28 00 46 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 47 00 ] [ 00 20 00 B1 ]
bitbang_cmd(): [ 28 00 47 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 48 00 ] [ 00 20 00 01 ]
#bitbang_cmd(): [ 28 00 48 00 ] [ 00 28 00 C0 ]
bitbang_cmd(): [ 20 00 49 00 ] [ 00 20 00 1D ]
bitbang_cmd(): [ 28 00 49 00 ] [ 00 28 00 92 ]
bitbang_cmd(): [ 20 00 4A 00 ] [ 00 20 00 A0 ]
bitbang_cmd(): [ 28 00 4A 00 ] [ 00 28 00 30 ]
#bitbang_cmd(): [ 20 00 4B 00 ] [ 00 20 00 B1 ]
bitbang_cmd(): [ 28 00 4B 00 ] [ 00 28 00 07 ]
bitbang_cmd(): [ 20 00 4C 00 ] [ 00 20 00 E1 ]
bitbang_cmd(): [ 28 00 4C 00 ] [ 00 28 00 F7 ]
bitbang_cmd(): [ 20 00 4D 00 ] [ 00 20 00 0E ]
#bitbang_cmd(): [ 28 00 4D 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 4E 00 ] [ 00 20 00 67 ]
bitbang_cmd(): [ 28 00 4E 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 4F 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 4F 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 50 00 ] [ 00 20 00 7A ]
bitbang_cmd(): [ 28 00 50 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 51 00 ] [ 00 20 00 0C ]
bitbang_cmd(): [ 28 00 51 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 52 00 ] [ 00 20 00 00 ]
#bitbang_cmd(): [ 28 00 52 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 53 00 ] [ 00 20 00 8F ]
bitbang_cmd(): [ 28 00 53 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 54 00 ] [ 00 20 00 84 ]
bitbang_cmd(): [ 28 00 54 00 ] [ 00 28 00 B9 ]
#bitbang_cmd(): [ 20 00 55 00 ] [ 00 20 00 87 ]
bitbang_cmd(): [ 28 00 55 00 ] [ 00 28 00 B9 ]
bitbang_cmd(): [ 20 00 56 00 ] [ 00 20 00 8E ]
bitbang_cmd(): [ 28 00 56 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 57 00 ] [ 00 20 00 8A ]
#bitbang_cmd(): [ 28 00 57 00 ] [ 00 28 00 B9 ]
bitbang_cmd(): [ 20 00 58 00 ] [ 00 20 00 08 ]
bitbang_cmd(): [ 28 00 58 00 ] [ 00 28 00 95 ]
bitbang_cmd(): [ 20 00 59 00 ] [ 00 20 00 0A ]
bitbang_cmd(): [ 28 00 59 00 ] [ 00 28 00 C0 ]
#bitbang_cmd(): [ 20 00 5A 00 ] [ 00 20 00 2A ]
bitbang_cmd(): [ 28 00 5A 00 ] [ 00 28 00 E5 ]
bitbang_cmd(): [ 20 00 5B 00 ] [ 00 20 00 00 ]
bitbang_cmd(): [ 28 00 5B 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 5C 00 ] [ 00 20 00 00 ]
#bitbang_cmd(): [ 28 00 5C 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 5D 00 ] [ 00 20 00 00 ]
bitbang_cmd(): [ 28 00 5D 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 5E 00 ] [ 00 20 00 00 ]
bitbang_cmd(): [ 28 00 5E 00 ] [ 00 28 00 00 ]
#bitbang_cmd(): [ 20 00 5F 00 ] [ 00 20 00 00 ]
bitbang_cmd(): [ 28 00 5F 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 60 00 ] [ 00 20 00 00 ]
bitbang_cmd(): [ 28 00 60 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 61 00 ] [ 00 20 00 21 ]
#bitbang_cmd(): [ 28 00 61 00 ] [ 00 28 00 50 ]
bitbang_cmd(): [ 20 00 62 00 ] [ 00 20 00 C1 ]
bitbang_cmd(): [ 28 00 62 00 ] [ 00 28 00 F7 ]
bitbang_cmd(): [ 20 00 63 00 ] [ 00 20 00 01 ]
bitbang_cmd(): [ 28 00 63 00 ] [ 00 28 00 97 ]
#bitbang_cmd(): [ 20 00 64 00 ] [ 00 20 00 00 ]
bitbang_cmd(): [ 28 00 64 00 ] [ 00 28 00 97 ]
bitbang_cmd(): [ 20 00 65 00 ] [ 00 20 00 A1 ]
bitbang_cmd(): [ 28 00 65 00 ] [ 00 28 00 F7 ]
bitbang_cmd(): [ 20 00 66 00 ] [ 00 20 00 08 ]
#bitbang_cmd(): [ 28 00 66 00 ] [ 00 28 00 95 ]
bitbang_cmd(): [ 20 00 67 00 ] [ 00 20 00 1F ]
bitbang_cmd(): [ 28 00 67 00 ] [ 00 28 00 93 ]
bitbang_cmd(): [ 20 00 68 00 ] [ 00 20 00 0E ]
bitbang_cmd(): [ 28 00 68 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 69 00 ] [ 00 20 00 53 ]
bitbang_cmd(): [ 28 00 69 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 6A 00 ] [ 00 20 00 1F ]
bitbang_cmd(): [ 28 00 6A 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 6B 00 ] [ 00 20 00 18 ]
#bitbang_cmd(): [ 28 00 6B 00 ] [ 00 28 00 B9 ]
bitbang_cmd(): [ 20 00 6C 00 ] [ 00 20 00 15 ]
bitbang_cmd(): [ 28 00 6C 00 ] [ 00 28 00 B9 ]
bitbang_cmd(): [ 20 00 6D 00 ] [ 00 20 00 1B ]
bitbang_cmd(): [ 28 00 6D 00 ] [ 00 28 00 B9 ]
#bitbang_cmd(): [ 20 00 6E 00 ] [ 00 20 00 84 ]
bitbang_cmd(): [ 28 00 6E 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 6F 00 ] [ 00 20 00 91 ]
bitbang_cmd(): [ 28 00 6F 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 70 00 ] [ 00 20 00 0E ]
#bitbang_cmd(): [ 28 00 70 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 71 00 ] [ 00 20 00 59 ]
bitbang_cmd(): [ 28 00 71 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 72 00 ] [ 00 20 00 18 ]
bitbang_cmd(): [ 28 00 72 00 ] [ 00 28 00 B8 ]
#bitbang_cmd(): [ 20 00 73 00 ] [ 00 20 00 15 ]
bitbang_cmd(): [ 28 00 73 00 ] [ 00 28 00 B8 ]
bitbang_cmd(): [ 20 00 74 00 ] [ 00 20 00 1B ]
bitbang_cmd(): [ 28 00 74 00 ] [ 00 28 00 B8 ]
bitbang_cmd(): [ 20 00 75 00 ] [ 00 20 00 84 ]
#bitbang_cmd(): [ 28 00 75 00 ] [ 00 28 00 EF ]
bitbang_cmd(): [ 20 00 76 00 ] [ 00 20 00 91 ]
bitbang_cmd(): [ 28 00 76 00 ] [ 00 28 00 E0 ]
bitbang_cmd(): [ 20 00 77 00 ] [ 00 20 00 0E ]
bitbang_cmd(): [ 28 00 77 00 ] [ 00 28 00 94 ]
#bitbang_cmd(): [ 20 00 78 00 ] [ 00 20 00 59 ]
bitbang_cmd(): [ 28 00 78 00 ] [ 00 28 00 00 ]
bitbang_cmd(): [ 20 00 79 00 ] [ 00 20 00 F1 ]
bitbang_cmd(): [ 28 00 79 00 ] [ 00 28 00 CF ]
bitbang_cmd(): [ 20 00 7A 00 ] [ 00 20 00 F8 ]
#bitbang_cmd(): [ 28 00 7A 00 ] [ 00 28 00 94 ]
bitbang_cmd(): [ 20 00 7B 00 ] [ 00 20 00 FF ]
bitbang_cmd(): [ 28 00 7B 00 ] [ 00 28 00 CF ]
# | 100% 0.08s
avrdude: verifying ...
avrdude: 248 bytes of flash verified
bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]
bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]
bitbang_cmd(): [ 50 00 00 00 ] [ 00 50 00 62 ]
avrdude: safemode: lfuse reads as 62
bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]
bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]
bitbang_cmd(): [ 58 08 00 00 ] [ 00 58 08 D9 ]
avrdude: safemode: hfuse reads as D9
bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]
bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]
bitbang_cmd(): [ 50 08 00 00 ] [ 00 50 08 FF ]
avrdude: safemode: efuse reads as 7
avrdude: safemode: Fuses OK
avrdude done. Thank you.
Any help would be appreciated.
Thanks,
Chuck