- Fri Jun 03, 2011 1:15 pm
#128245
here is ,if condition to compare between constant temperature(Tl,Th)and the readable temperature T.
the lamp didn't respond to change in T .it doesn't switch on if T below the range or off when it is out of range
the lamp didn't respond to change in T .it doesn't switch on if T below the range or off when it is out of range
Code: Select all
#include <stdio.h>
#include <avr/io.h>
#include <avr/pgmspace.h>
#include <avr/interrupt.h>
#include <util/delay.h>
#include "lcd_lib.h"
//adjust LCDsendChar() function for stream
static int LCDsendstream(char c, FILE *stream);
//----set output stream to LCD-------
static FILE lcd_str = FDEV_SETUP_STREAM(LCDsendstream, NULL, _FDEV_SETUP_WRITE);
void delay1s(void);
void adc_init(void);
void adc_start_conversion(uint8_t);
static int LCDsendstream(char c , FILE *stream);
void init(void);
void init_interrupt0(void);
//current channel
uint8_t ch;
volatile uint16_t temp_current;
volatile uint8_t temp_min=20;
volatile uint8_t temp_max=27;
char x,j;
//strings for LCD stored in Flash memory
const uint8_t temp[] PROGMEM="temp:\0";
const uint8_t celsuis[] PROGMEM="C \0";
const uint8_t enterlowtemp[] PROGMEM="enterlowtemp\0";
const uint8_t enterHItemp[] PROGMEM="enterHItemp\0";
const uint8_t MENU[] PROGMEM="MENU\0";
const uint8_t UP[] PROGMEM="UP\0";
const uint8_t OK[] PROGMEM="OK\0";
const uint8_t Tl[] PROGMEM="Tl=\0";
const uint8_t Th[] PROGMEM="Th=\0";
const uint8_t CLRROW[] PROGMEM=" \0";
const uint8_t *LCDXY[] ={
temp, //for ADC0
enterlowtemp,Tl,enterHItemp,Th,MENU,UP,OK};
// ADC module initialization
//
//*****************************************************************************
void adc_init(void)
{
//select reference voltage
//AVCC with external capacitor at AREF pin
ADMUX|=(0<<REFS1)|(1<<REFS0);
//set prescaller and enable ADC
ADCSRA|=(1<<ADEN)|(1<<ADIE);//enable ADC with dummy conversion
//set sleep mode for ADC noise reduction conversion
//set_sleep_mode(SLEEP_MODE_ADC);
}
//*****************************************************************************
//
// ADC single conversion routine
//
//*****************************************************************************
void adc_start_conversion(uint8_t channel)
{
//remember current ADC channel;
ch=channel;
//set ADC channel
ADMUX=(ADMUX&0xF0);
//Start conversionio with Interupt after conversion
//enable global interrupts
//continue infinitely
sei();
ADCSRA |= (1<<ADSC)|(1<<ADIE);
}
//
// delay 1s
//
//*****************************************************************************
//delay 1s
void delay1s(void)
{
uint8_t i;
for(i=0;i<100;i++)
{
_delay_ms(10);
}
}
//*****************************************************************************
//
// Set LCD stream function
//
//*****************************************************************************
static int LCDsendstream(char c , FILE *stream)
{
LCDsendChar(c);
return 0;
}
//*****************************************************************************
//
// init AVR
//
//*****************************************************************************
void init(void)
{
//init stream
stdout = &lcd_str;
//init LCD
LCDinit();//init LCD bit, dual line, cursor right
LCDclr();//clears LCD
LCDGotoXY(0, 0);//Cursor Home
//Init ADC
adc_init();
}
//
// ADC conversion complete service routine
//
//*****************************************************************************
ISR(ADC_vect)
{
uint16_t adc_value;
adc_value = (((unsigned long)ADC*500+512)/1024);
CopyStringtoLCD(CLRROW, 0, ch );
CopyStringtoLCD(LCDXY[(ch)], 0, ch );
//LCDGotoXY(6, 0);
printf("%d", adc_value);
CopyStringtoLCD(celsuis,9, 0);
LCDGotoXY(7, 0);
LCDsendChar(0xDF);
temp_current=adc_value;
}
//*****************************************************************************
//
// run analog digital converter, timer.
//
//*****************************************************************************
int main(void)
{
init();
printf("temp.controller");
DDRB |= 0x10;
delay1s();
while(1)//loop demos
{
//read lm35
adc_start_conversion(0);
_delay_ms(50);
CopyStringtoLCD(MENU, 12, 1);
if (((temp_min<temp_current)&&(temp_current<temp_max))||(temp_current>temp_max)) // compare temperature
{
PORTB |= 0x00; //make Bit 4 of PORTB low to turn LED off
}
else if (temp_current<temp_min)//&&(PINC & 0x04))// if temp< low & press ok
{
PORTB |= 0x10; //make Bit 4 of PORTB High to turn LED on
}
init_interrupt0();
}
return 0;
}