- Mon Apr 11, 2011 8:24 pm
#125150
Hey guys! I want to thank you in advance for any help you can offer.
I'm running Win7 x64
I just received my AVR Pocket Programmer and have set-up AVR dude (version 5.10). I have successfully written one test .hex file to my Attiny44 but am now trying to write the code I got from this Mechanized Android Figure tutorial (http://www.instructables.com/id/Mechani ... /Software/) I'm following. I exported the source code to a .hex file with Hex Workshop. When I try to flash it I receive the following error.
avrdude: ERROR: address 0x1010 out of range at line 257 of /android8.hex
I've read that the issue I'm having should be fixed in version 5.10 of avrdude but apparently that is not the case.
From http://www.avrfreaks.net/index.php?name ... 65&start=0
Thanks!
I'm running Win7 x64
I just received my AVR Pocket Programmer and have set-up AVR dude (version 5.10). I have successfully written one test .hex file to my Attiny44 but am now trying to write the code I got from this Mechanized Android Figure tutorial (http://www.instructables.com/id/Mechani ... /Software/) I'm following. I exported the source code to a .hex file with Hex Workshop. When I try to flash it I receive the following error.
avrdude: ERROR: address 0x1010 out of range at line 257 of /android8.hex
I've read that the issue I'm having should be fixed in version 5.10 of avrdude but apparently that is not the case.
From http://www.avrfreaks.net/index.php?name ... 65&start=0
Sorry, I had to re-release AVRDUDE, so there's now version 5.10 out.Any ideas on how to fix this?
The reason was that 5.9 had a serious bug in handling intel hex files
with more than 128 KiB of flash contents. This has been fixed.
Thanks!