- Fri Mar 10, 2006 8:35 pm
#10904
If Olimex is around, maybe he can shed some light: On the Atmega128 header board, there is a pullup resistor on the PEN pin. According to the datasheet, this pin is pulled up internally, and is used to enter SPI programming mode when pulled low. So is that resistor really necessary? Or is it just there so that, when I pull the pin low I don't blow up the battery
Also, the datasheet says that, if I want to use the ADC, I need to connect AVCC to VCC through a "low-pass" filter. 1) what the heck is a "low-pass filter"? and 2) is there a way to do this with the header board? It looks like AVCC is already connected to VCC...
Also, the datasheet says that, if I want to use the ADC, I need to connect AVCC to VCC through a "low-pass" filter. 1) what the heck is a "low-pass filter"? and 2) is there a way to do this with the header board? It looks like AVCC is already connected to VCC...