- Sun Sep 26, 2010 5:39 pm
#110204
Hi everbody. I recently got my order from sparkfun and was super excited to start messing with everything it came with. One of the things I ordered was a shift register (specifically the Shift Register 8-Bit - 74HC595) Now I was just trying to mess around with it, by getting it light up 8 leds in a pattern. The problem is that I cant even seem to get it to work. I have Vcc and ground hooked up to power and ground respectively. I have the serial input pin hooked up to the avr as well as the clock pin and the latch pin. Now I thought that you made the serial input pin either high or low(to represent a 1 or a 0) and then you set the clock pin high. That shifts in the first bit. You would do that 8 times and then set the latch pin high and it would light up the leds, but i cant seem to get that to work.