- Mon Apr 26, 2010 11:34 am
#99477
I'm working on a project with a Arduino Diecimila, ADXL335 Accelerometer, and the WiFly
shield.
I have used the WiFly Wireless Talking SpeakJet Server (http://www.sparkfun.com/commerce/tutori ... als_id=158) as a primary guide to understanding and communicating to and from the Artduino with the WiFly shield.
Everything has worked great as far as connecting to our WiFi network, communicating to and from the Arduino over this WiFi connection and getting a basic HTML page from the Arduino.
What I have not been able to do so far is successfully hit a web server FROM the arduino.
I have tried to use the open command (a WiFly command) to open a connection to a server and then send the test of an HTTP request which I then close. I have tried this manually through a serial connection to the arduino and in my sketch.
Here is the code snippet from that sketch I am trying to use as a test:
Serial.println("Opening Connection to HTTP Server");
SPI_Uart_print("$$$");
delay(500);
SPI_Uart_println("open 172.16.48.195 80");
delay(3000);
Serial.println("Sending GET request to server");
SPI_Uart_println("GET /ard/test.php?arvalue=arduinotest HTTP/1.1");
delay(800);
SPI_Uart_print("$$$");
delay(500);
Serial.println("Closing Connection to HTTP Server");
SPI_Uart_println("close");
delay(500);
SPI_Uart_println("exit");
delay(500);
Flush_RX();
The functions used in this code are from the tutorial referenced above from Sparkfun.
I'm sure there is something I'm missing but I can not see any evidence in my apache logs that any attempts are being received from the arduino.
I also can not find any additional indications through the WiFly docs as to other approaches or options.
Any ideas or guidance is very welcomed.
Thanks!!
shield.
I have used the WiFly Wireless Talking SpeakJet Server (http://www.sparkfun.com/commerce/tutori ... als_id=158) as a primary guide to understanding and communicating to and from the Artduino with the WiFly shield.
Everything has worked great as far as connecting to our WiFi network, communicating to and from the Arduino over this WiFi connection and getting a basic HTML page from the Arduino.
What I have not been able to do so far is successfully hit a web server FROM the arduino.
I have tried to use the open command (a WiFly command) to open a connection to a server and then send the test of an HTTP request which I then close. I have tried this manually through a serial connection to the arduino and in my sketch.
Here is the code snippet from that sketch I am trying to use as a test:
Serial.println("Opening Connection to HTTP Server");
SPI_Uart_print("$$$");
delay(500);
SPI_Uart_println("open 172.16.48.195 80");
delay(3000);
Serial.println("Sending GET request to server");
SPI_Uart_println("GET /ard/test.php?arvalue=arduinotest HTTP/1.1");
delay(800);
SPI_Uart_print("$$$");
delay(500);
Serial.println("Closing Connection to HTTP Server");
SPI_Uart_println("close");
delay(500);
SPI_Uart_println("exit");
delay(500);
Flush_RX();
The functions used in this code are from the tutorial referenced above from Sparkfun.
I'm sure there is something I'm missing but I can not see any evidence in my apache logs that any attempts are being received from the arduino.
I also can not find any additional indications through the WiFly docs as to other approaches or options.
Any ideas or guidance is very welcomed.
Thanks!!