- Sat Nov 12, 2005 4:35 pm
#7874
Hi,
I have the same problem as henrik told you guys.
I cannot get the avr studio to connect to the board.
Here is the deal:
got the usb avr jtag ice.
installed the driver and configured it on port 2.
connected the usb jtag ice to computer with a usb cable.
on the other side, i connect the jtag ice to ATMEL BUTTERFLY using the cable provided with the usb jtag ice. I made sure the pins mach ( the pins are soldered on back of the butterfly....).
Then, I connect external power( provided by an adaptor), to the board.. it has voltage of 4 volts.
Then goto AVR studio and try to connect to the thing.. ( I have tried both auto and com2) ....
It gives me the errro... Also, in non of the steps above the LED on the jtag ice comes on...
What do you guys suggest?
I would like to mention that, the usb cable that i used, I bought it, like a year ago. However, I checked the voltages on the USB JTAG ICE to see if its powered up by usb, and it was...
I have the same problem as henrik told you guys.
I cannot get the avr studio to connect to the board.
Here is the deal:
got the usb avr jtag ice.
installed the driver and configured it on port 2.
connected the usb jtag ice to computer with a usb cable.
on the other side, i connect the jtag ice to ATMEL BUTTERFLY using the cable provided with the usb jtag ice. I made sure the pins mach ( the pins are soldered on back of the butterfly....).
Then, I connect external power( provided by an adaptor), to the board.. it has voltage of 4 volts.
Then goto AVR studio and try to connect to the thing.. ( I have tried both auto and com2) ....
It gives me the errro... Also, in non of the steps above the LED on the jtag ice comes on...
What do you guys suggest?
I would like to mention that, the usb cable that i used, I bought it, like a year ago. However, I checked the voltages on the USB JTAG ICE to see if its powered up by usb, and it was...
Ashkan Ziabakhsh Deylami