ChaosBuster wrote: ↑Wed Jun 27, 2018 11:23 am
In the Tasks (section 4) there are references to at least two task instances for either Pickup, Transport or Deliver. In the Scoring (section 6) there are references to only one scoring and max points for these tasks. Does that mean there will not be full points for all the boxes that are referenced in the Tasks?
You're right, that was unclear. The intent is to repeat the points given for each type of task without repeating the verbiage.
Here's a full breakdown of max points by task ( manual / autonomous )
- Start: 10 / 30
- Pickup (up to two boxes): 20 / 100
- Transport to Production (up to two boxes): 20 / 60
- Deliver to Manufacture (up to two boxes): 20 / 100
- Pickup Finished Product: 10 / 50
- Test: 10
- Transport to Warehouse: 10 / 30
- Deliver to Destination Shelf: 10 / 50
- Get Back to Work 0 / 0
Now that I'm reading it again, it was worded pretty badly. My apologies. I'll post the official score sheet so judges and contestants are on the same page.
ChaosBuster wrote: ↑Wed Jun 27, 2018 12:49 pm
QUESTION: Can the two Raw Material boxes be stacked or placed in any way as long as they are within the input area of the Pick-n-Place?
Yes. The pick-n-place is a super advanced machine and can handle anything that lands within its input area.