Page 1 of 3
Have you considered ScreenKeys?
Posted: Sat Sep 29, 2007 8:11 pm
by MarkS
I got a sample of the RGB24 from
www.ScreenKeys.com and have designed a small protoboard that holds one switch, includes two surface mount pull-up resistors and uses .1" pin spacing on a staggered grid for solderless breadboard mounting. The problem is that the board is less than 1" square and making only one would be cost prohibitive. The switch is really novel and easy to control though. It would be nice to have a prototyping system for these buttons. ScreenKeys makes their own, but the design is not very realistic. Why use a 48-pin DIP 8051 microcontroller for a couple of switches when you can get the same effect from a smaller SMD controller?
Posted: Sun Sep 30, 2007 7:41 am
by ttabbal
You could send the board through BatchPCB. I had a 4sqin board done for about $30. Hard to beat that price for a full board. That would get the PCB cost down and you can design it to be whatever you want.
Cool switches though. I might have to get a sample to mess with. Might be an interesting product for SFE to sell...
Posted: Sun Sep 30, 2007 8:30 am
by Heffo
I could find a use for a few of those switches myself
Posted: Sun Sep 30, 2007 12:42 pm
by MarkS
This is the breakout board and schematic:
As you can see, its very simple, but very small. The board measures 24mmx23mm. There are no mounting holes. Mounting would be accomplished with the 6 pin headers. The two pull-up resistors are 0805 package SMD.
The control board will be a little bit more complicated, but not by much.
Posted: Sun Sep 30, 2007 1:24 pm
by Philba
cool product. how liberal are they with samples?
What is the cost per switch in small quantities? I couldn't find the products on the disti web sites they point to.
For a one-off, I'd just use vector board and axial resistors. not a lot of work to wire up.
Posted: Mon Oct 01, 2007 8:02 am
by phalanx
Philba wrote:cool product. how liberal are they with samples?
What is the cost per switch in small quantities?
I just sent a sample request to them using my work information and also requested their pricing tables. I'll send you the info once I receive it.
-Bill
Posted: Mon Oct 01, 2007 9:10 am
by MarkS
Philba wrote:cool product. how liberal are they with samples?
What is the cost per switch in small quantities? I couldn't find the products on the disti web sites they point to.
They sent me one switch, so they are not very liberal.
Their distributor's web sites suck. I don't know if they sell them only in volume, or what the pricing is per switch. You are forced to deal with their sales staff, which means getting small quantities may be a hassle.
Posted: Mon Oct 01, 2007 9:46 pm
by wiml
NKK has a product like this also; their brand name is "SmartSwitch". But they also seem to be impossible to buy. You can buy an evaluation kit from Mouser with 2 switches for $250. I'm guessing the switches themselves are more expensive than I'm willing to pay just for the niftiness factor.
Posted: Tue Oct 02, 2007 10:49 am
by phalanx
I just received a few quotes from one of their sales people.
The RGB version of the switch is about 20 Euro in 1-100 quantities.
The RG version is 14 Euro.
Development boards are as follows:
RGB microcontroller kit with 2 buttons = 75 Euro
RG microcontroller kit with 2 buttons = 65 Euro
Too bad the dollar isn't that strong at the moment because those are very reasonable prices in my book.
-Bill
Posted: Thu Oct 04, 2007 7:01 am
by Encryptic
I'm inclined to say that these have a pretty cool 'wow' factor, but they're out of my price range...
E3-Keys
Posted: Thu Oct 11, 2007 9:52 am
by roland_weimer
You may want to check out
www.e3-keys.com as well - higher resolution, over 10,000 calibrated RGB colors, extended command set, etc.
Posted: Thu Oct 11, 2007 10:19 am
by busonerd
Just as a heads up - we have a bunch of the screenkeys coming in - so keep an eye out on the storefront.
Cheers,
--David Carne
Posted: Thu Oct 11, 2007 10:20 am
by brennen
David-
Any word on how much they'll be in single quantities?
Posted: Thu Oct 11, 2007 10:23 am
by busonerd
Not yet - I don't make pricing calls, was just giving you guys a heads up on our progress.
Cheers,
--David Carne
Posted: Thu Oct 11, 2007 11:52 pm
by MarkS
busonerd wrote:Just as a heads up - we have a bunch of the screenkeys coming in - so keep an eye out on the storefront.
Cheers,
--David Carne
Wow! That was fast!