SparkFun Forums 

Where electronics enthusiasts find answers.

Have a good idea for a new product for SFE or Olimex? Let us know!
By AgroMe
#196469
Hi there!

Idea for a product: microSD to Standard SD Adapter

Would be like putting together products 9419 and 11468

There are some cables out there for about $4-10 but they are too long (48-70 cm) and this probably affects the signal. I hacked a converter using your products 9419 and 11468 and had to shield the cables else it would not work, so I don't trust those "GPS" cables will work very well.

Why is this product important?

There reasonably priced industrial SLC SD Cards (for example Cactus https://www.cactus-tech.com which have 100,000 write cycles lifetime per block!). These SD cards are ideal to expand embedded application that have microSD, but S.M.A.R.T. is not usually available in the microSD format, but it's available in the Cactus full size SD for example.

The adapter could be rigid and simple such as the microSD sniffer 9419, but it would also be cool if it had a flexible shielded cable so the full size SD could be mounted with posts and screws. Maybe you can make both versions like a budget one (rigid PCB like the 9419) or more expensive option with shielded flexible cable. Both should have a mounting hole to avoid the thing from moving.

Anyway I have attached the 9419 + 11468 and works like a charm although without the shielding it doesn't work at all. I used aluminium tape that is used for heat ducting (dryer, furnace, etc.).

Thanks,
Alex
You do not have the required permissions to view the files attached to this post.
long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]