New product Ideas

Have a good idea for a new product for SFE or Olimex? Let us know!

Moderator: phalanx

Post Reply
User avatar
sparky
Site Admin
Posts: 1342
Joined: Mon May 05, 2003 6:02 pm
Location: Colorado
Contact:

New product Ideas

Post by sparky » Mon May 05, 2003 6:34 pm

We've got some fun stuff up our sleeve - all to be rolled out this summer.

Have you got an idea for something that needs to get added to the site? Post it and let us know!

-Sparky

Ken
Posts: 30
Joined: Fri Jul 02, 2004 11:29 am
Location: London

New Product Idea PIC to Compact Flash Dev Board

Post by Ken » Sat Jul 03, 2004 9:48 am

Hi Sparky,

How about a simple experimenter's board with a PIC16F877A (or 18F452) and a Compact Flash Interface- it takes about 17 lines of I/O to implement.

With this you have the basis of many interesting products, MP3 player, telephone answering machine, file reader etc.




Ken

Guest

Post by Guest » Mon Jul 12, 2004 7:48 am

Hi,
how about something for educational purposes:

A Variation of the AVR-MT-128, but only single-sided (mountability) and with a SOCKETED processor, if it reaches its end of life, due to excessive amount of reprogramming it. The Processor can range from 16 - 128 (for JTAG). Even the 10K (Flash) / 100K (EEPROM) read/write cycles (e.g. mega16 / mega128) can be done relatively fast, especially in an educational context, where beginners have to use the board ;)

Oh, another thing i almost forgot: Every Pin of the Processor should be available for external connection, not only the unused (maybe with jumpers to choose onboard/external use, like on http://www.unesols.com/products_pages/A ... atures.htm)

The last thing on the wishlist for that board is: some 7-segment option.

-------

Another board: Just some 7-segments and a RS232 connector (and a preprogrammed processor to control the 7-segments based on the data it gets via the RS232), so another board can use its connector-pins freely, with only the the RS232 pins needed to control xy 7-segment-displays.

greets
Bodo

User avatar
sparky
Site Admin
Posts: 1342
Joined: Mon May 05, 2003 6:02 pm
Location: Colorado
Contact:

Post by sparky » Tue Jul 13, 2004 11:00 am

That's a beautiful AVR board. We try to keep the development boards universal so that you can add anything you want. No sense in buying an entire layout if all you are going to use is 30% of it.

-Nathan

bloody-orc
Posts: 5
Joined: Thu Aug 19, 2004 9:41 am

Post by bloody-orc » Fri Aug 20, 2004 12:09 pm

well if you want to make something a starter paack for lets say for PIC is a good idea. :wink:

It should include : PIC, some kind of a board to program and make some projects on it (blink a led etc.), softwere on cd(s) to program that PIC and some instructions how to do it

and this all in one pacage...

i hope that you got the idea.

Post Reply