Ideal Diode Breakout

Have a good idea for a new product for SFE or Olimex? Let us know!

Moderator: phalanx

Post Reply
DrT
Posts: 1
Joined: Sat Nov 26, 2011 11:34 am

Ideal Diode Breakout

Post by DrT » Sat Nov 26, 2011 11:43 am

I frequently have a need to prototype redundant power supply systems. For example, having two lithium ion battery packs powering a circuit with a plug-in charger. When the charger is plugged in, ideally, the batteries will isolate from the circuit and charge while the charger supplies power to the circuit.

Even better is to have three lines on the charger. One to power the circuit, one to charge battery pack number 1, and one to charge battery pack number 2. By isolating the battery packs from each other and from the main circuit charging can be done more rapidly and with greater safety.

The common technique for isolation is by diode ORing the batteries. However, this is pretty power hungry.

There exist some very nice devices used to create an ideal (30 mOhm) diode for this purpose (e.g., Linear Technologies, LTC4358 - http://cds.linear.com/docs/Datasheet/4358fa.pdf). These devices are invariably surface mount and would be far easier to use if you would create a breakout board for them.

Thanks for taking a look.

DrT

serveurperso
Posts: 3
Joined: Thu Apr 07, 2011 11:45 pm
Location: France Paris
Contact:

Re: Ideal Diode Breakout

Post by serveurperso » Wed Jun 06, 2018 11:44 pm

+1 need an ideal diode breakout to protect any charge connector on robot.
https://www.serveurperso.com/?page=robot - 8 cameras, UHF downlink, PIC32 bare-metal + external NodeJS server + H.264

http://www.serveurperso.com:8080 - 3 cameras, PIC32 bare-metal + embedded web GUI/Wi-Fi/captive portal/NodeJS server + H.264

Post Reply