SparkFun Forums 

Where electronics enthusiasts find answers.

Have a good idea for a new product for SFE or Olimex? Let us know!
By DrT
#136200
I frequently have a need to prototype redundant power supply systems. For example, having two lithium ion battery packs powering a circuit with a plug-in charger. When the charger is plugged in, ideally, the batteries will isolate from the circuit and charge while the charger supplies power to the circuit.

Even better is to have three lines on the charger. One to power the circuit, one to charge battery pack number 1, and one to charge battery pack number 2. By isolating the battery packs from each other and from the main circuit charging can be done more rapidly and with greater safety.

The common technique for isolation is by diode ORing the batteries. However, this is pretty power hungry.

There exist some very nice devices used to create an ideal (30 mOhm) diode for this purpose (e.g., Linear Technologies, LTC4358 - http://cds.linear.com/docs/Datasheet/4358fa.pdf). These devices are invariably surface mount and would be far easier to use if you would create a breakout board for them.

Thanks for taking a look.

DrT
long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]