- Sat May 14, 2011 9:23 pm
#127204
This post is a request for Sparkfun to either manufacture or acquire a series of Arduino boards compatible with the ANDROID ADK. I would hope that the first would be a revision on the Arduino MEGA 2560. These would be similar to the board at http://www.rt-shop.sakura.ne.jp/rt-shop ... ts_id=2731. The RT-ADK board has the USB HOST chip MAX3421E integrated on the board. It would also be nice to see a full USB-B off of the FTDI chip in place of the micro USB board. I realize that there is a shield for this but it would be nice for it to be all in one to allow for other shields such as the ethernet shield to be used in conjunction with cases like the Arduino crib. I look forward to the feedback on this post.