- Mon Feb 06, 2006 8:47 am
#9553
I'm working on a project that will need several (4) 2x5 0.1" headers. At least two of them really need to be 0.1" for standard ICSP and JTAG connectors. I'd like to use 2mm headers to save space. A breakout board with a double row of 2MM pitch holes on one end connected to a double row of 0.1" pitch holes on the other end would be great. For flexibility it could be 2X10 (or even wider) as long as I can just plug in the width I need.
I realize this is a fairly trivial request and I could whip up a board to do this myself. But if I need a few of these I figure someone else might too!
I realize this is a fairly trivial request and I could whip up a board to do this myself. But if I need a few of these I figure someone else might too!