- Wed May 04, 2005 12:55 pm
#4768
Would it be possible to have something like the DLP-USB245M, but with more bandwidth?
I really like the FIFO interface on the 245M for it's simplicity, but would love something a little faster. I don't need USB 2.0's theoretical max of 480Mbps, but 20Mbps+ would be very much appreciated. A 16-bit wide data path instead of 8-bit wide would be okay, or even 32-bits wide if that would allow more throughput. Since the DLP-USB245M is IIRC under $20, under $50 for the uber-high-speed replacement would be ideal.
Thanks.
I really like the FIFO interface on the 245M for it's simplicity, but would love something a little faster. I don't need USB 2.0's theoretical max of 480Mbps, but 20Mbps+ would be very much appreciated. A 16-bit wide data path instead of 8-bit wide would be okay, or even 32-bits wide if that would allow more throughput. Since the DLP-USB245M is IIRC under $20, under $50 for the uber-high-speed replacement would be ideal.
Thanks.