espcomm errors after updating to macOS 10.13.1 High Sierra

A place to hang out and chat with other like minded tinkerers

Moderators: phalanx, TS-Tim

Post Reply
TS22082
Posts: 4
Joined: Tue Nov 14, 2017 11:30 am

espcomm errors after updating to macOS 10.13.1 High Sierra

Post by TS22082 » Tue Nov 14, 2017 11:44 am

Im all over the place trying to get the ESP8266 thing dev to accept uploads again. Really hoping im in the right place to get this figured out, if you have another place to look i'de really appreciate the advice.

I believe updating to High Sierra caused the problem because code that was working RIGHT before the update, do not upload anymore. I even tried uploading the sample blinky program and it wont upload to the board either. I used 2 different USB cables to make sure that wasn't the problem.

Module: Sparkfun ESP8266 Thing Dev
CPU Frequency: 80Mhz
Upload Using: usbserial-DN031130

The errors I'm getting when trying to upload a sketch to the board:

Code: Select all

An error occurred while uploading the sketch Uploading 228336 bytes from /var/folders/vm/7zhkws111z575vj68kz3wzkw0000gn/T/arduino_build_776513/blickyESP8266.ino.bin to flash at 0x00000000 

Code: Select all

warning: espcomm_send_command: didn't receive command response 

Code: Select all

warning: espcomm_send_command(FLASH_DOWNLOAD_DATA) failed

Code: Select all

warning: espcomm_send_command: wrong direction/command: 0x01 0x03, expected 0x01 0x04

Code: Select all

error: espcomm_upload_mem failed

theropod
Posts: 91
Joined: Tue Sep 20, 2016 11:12 am

Re: espcomm errors after updating to macOS 10.13.1 High Sierra

Post by theropod » Tue Nov 14, 2017 4:00 pm

It is very much the Mac OS update causing this issue. Do a net search for the correct USB driver that will work with the Ardunio IDE and High Sierra, as a dime against a dollar says Apple has limited the USB porting in the last update. Apple has turned into control freaks dictating what users can and cannot do with their own equipment. After the iOS update to 11.0.3 ruined my iphone 6 plus I will never buy another Apple product. I have been a loyal user/owner since 1992.
16 years off the grid and lovin' it!

Post Reply