SparkFun Forums 

Where electronics enthusiasts find answers.

By Bartowskio
#192159
I am trying to build the following exponential converter circuit from the Thomas Henry "Making Music with the 3080 OTA" document.
Image
I understand from his text that this circuit may be ok for VCAs and VCFs but isn't ideal for tuning VCOs unless you can find an NPN-PNP Matched pair, which is very difficult to do. I'm not quite yet at the skill level to understand the matched pair expo converters using a differential amplifier setup of two matched PNP or NPN transistors, but I do understand this circuit and would like to see if I can use it for a simple VCO of about 4 octaves before I continue studying the more standard matched pair expo converters.

Question: Can I use two different kinds of NPN/PNPs to match, such as a 2N3906 and a 2SC945, or would the two transistors have to be complements of the same kind like the 2N3906-2N3904? I managed to find a 2N3906 and 2SC945 who's Vbe deltas are just about 2mV.
2n3906 transistor
Image
Can I use those in this circuit?