How to install one thermostat?Is there anyone use it ?

A place to hang out and chat with other like minded tinkerers

Moderator: phalanx

Post Reply
lerway
Posts: 5
Joined: Tue May 05, 2015 7:55 pm
Contact:

How to install one thermostat?Is there anyone use it ?

Post by lerway » Tue May 05, 2015 8:23 pm

How to install one thermostat(temperature controller)?Is there anyone use it for home brew .The device information like following:

Detailed Product Description
Measure range:-50~+99°C
Mounting size:71*29mm
Auto switch between refrigerating and heating
Retrun difference value
All-purpose Temperature Controller STC-1000:

Features:
Switch the modes between cool and heat; Control temperature by setting the temperature setting value and the difference value; Temperature calibration; Refrigerating control output delay protection; Alarm when temperature exceeds temperature limit or when sensor error.

Specification and Size:
1.Front panel size75(L)×34.5(W)mm;
2.Mounting size:71(L)×29(W)mm;
3.Product size75(L)×34.5(W)×85(D)mm;
4.sensor length2minclude the probe.

Technical Parameters:
1. Temperature measuring range: -50~99oC;
2. Resolution: 0.1°C; 3. Accuracy: ±1°C (-50~70°C);
4. Sensor error delay: 1 minute
5. Power supply: 110VAC±10%, 50/60Hz;
6. Power consumption: ≤3W;
7. Sensor: NTC sensor (1PC);
8. Relay contact capacity: Cool 10A/250VAC;Heat 10A/250VAC;
9. Ambient temperature: 0~60°C;
10.Storage temperature: -30~75°C;
11.Relative humidity: 20%~85% (No condensate).

User avatar
Ross Robotics
Support Volunteer
Posts: 2007
Joined: Thu Jun 07, 2012 9:33 pm
Contact:

Re: How to install one thermostat?Is there anyone use it ?

Post by Ross Robotics » Wed May 06, 2015 7:59 am

What do you mean install it? Do you mean how to connect it to a controller?
------------------------------------------------------------------------------------------------------------------------------------------------------------
//codlink
Available for circuit and PCB design, just PM me!

lerway
Posts: 5
Joined: Tue May 05, 2015 7:55 pm
Contact:

Re: How to install one thermostat?Is there anyone use it ?

Post by lerway » Wed May 06, 2015 7:06 pm

codlink wrote:What do you mean install it? Do you mean how to connect it to a controller?

Oh ,yes ,I don;t know how to connect it.
Smart life,smart home,happy home brew,click here to see more.https://www.facebook.com/pages/Inkbird/358784690993195

n1ist
Support Volunteer
Posts: 1038
Joined: Wed Mar 22, 2006 11:02 am

Re: How to install one thermostat?Is there anyone use it ?

Post by n1ist » Thu May 07, 2015 5:36 am

Look at the side of the STC-1000; the picture describes the connections. Also, do a google search for "STC-1000". There are many hits. This one http://brewprof.com/weekend-diy-homebre ... -stc-1000/ shows how to mount the controller in a box with two controlled outlets on the output.
This thread http://www.homebrewtalk.com/showthread.php?t=330427 goes into details on how to add relays to power larger loads.
/mike

lerway
Posts: 5
Joined: Tue May 05, 2015 7:55 pm
Contact:

Re: How to install one thermostat?Is there anyone use it ?

Post by lerway » Fri May 08, 2015 12:24 am

n1ist wrote:Look at the side of the STC-1000; the picture describes the connections. Also, do a google search for "STC-1000". There are many hits. This one http://brewprof.com/weekend-diy-homebre ... -stc-1000/ shows how to mount the controller in a box with two controlled outlets on the output.
This thread http://www.homebrewtalk.com/showthread.php?t=330427 goes into details on how to add relays to power larger loads.
/mike
:clap: :clap: :clap:

Thank you so much !
Smart life,smart home,happy home brew,click here to see more.https://www.facebook.com/pages/Inkbird/358784690993195

lerway
Posts: 5
Joined: Tue May 05, 2015 7:55 pm
Contact:

Re: How to install one thermostat?Is there anyone use it ?

Post by lerway » Thu May 14, 2015 8:52 pm

This videos tell us how to connect one PID temp. controller but I'd like to know how to connect one ITC-1000F

https://youtu.be/DZDkrR0Vhrc
Smart life,smart home,happy home brew,click here to see more.https://www.facebook.com/pages/Inkbird/358784690993195

User avatar
DanV
Posts: 393
Joined: Sat Apr 25, 2015 9:29 am

Re: How to install one thermostat?Is there anyone use it ?

Post by DanV » Fri May 15, 2015 12:17 pm


lerway
Posts: 5
Joined: Tue May 05, 2015 7:55 pm
Contact:

Re: How to install one thermostat?Is there anyone use it ?

Post by lerway » Thu May 21, 2015 10:43 pm

Thank you.
Smart life,smart home,happy home brew,click here to see more.https://www.facebook.com/pages/Inkbird/358784690993195

Post Reply