Stepper motor help

A place to hang out and chat with other like minded tinkerers

Moderator: phalanx

Post Reply
elbowrust
Posts: 2
Joined: Fri Mar 20, 2015 5:06 am

Stepper motor help

Post by elbowrust » Fri Mar 20, 2015 5:26 am

Hi all!
I have a stock pile of stepper motors which we normally throw away. I'm wondering if I could use these for a CNC application. Probably overkill but thought I would get your opinions.
Amatek HS 200 2231 0300
Max V 75
Rated phase current 3A
Holding torque 231 oz-in bipolar
1.8° step angle
NEMA 23 mounting config.

Any help would be appreciated.

jremington
Support Volunteer
Posts: 2324
Joined: Fri Jun 15, 2007 9:41 pm
Location: Eugene, Or

Re: Stepper motor help

Post by jremington » Fri Mar 20, 2015 8:25 am

There aren't any hobby-type stepping motor controllers capable of the full 3A/phase, but if reduced torque will do, the Pololu DRV8825 board will handle 1.5 amps/phase without additional cooling. Be sure to follow instructions for setting the current limit. https://www.pololu.com/product/2133

elbowrust
Posts: 2
Joined: Fri Mar 20, 2015 5:06 am

Re: Stepper motor help

Post by elbowrust » Fri Mar 20, 2015 6:53 pm

I don't need that much torque. They will be running the x and y axis on a laser engraver so there will be minimal resistance. Can I run these steppers at 15v .5A and still get the necessary speed and precision?

Post Reply