SparkFun Forums 

Where electronics enthusiasts find answers.

By wenganxiang
#179751
I got a Geeetech 3d-printer, and printed my first object. Here is how it’s made from ABS filament, and a lot of details about the model.

Start
Create 3D objects in reality, sounds difficult and magical. In the past, only factories can do it. But now it’s simple and the method is easy to understand.

A 3D model is cut into pieces or layers in computer, each layer is thinner than 1mm. Printing a layer is easy, just like painting with melting plastic, and then other layers upon it. It gets thicker and thicker and becomes the model you want.
QQ截图20150211154147.png
Grids
In fact, the model is not totally solid. As you can see grids in the model, especially in the middle(the edge is solid). I think the grid structure can save material, it’s lighter but also has required strength--solid doesn’t means strong all the time.
QQ截图20150211154216.png
Notes
Neighbor layers should be adhere to each other, however sometimes they are separated, because of unsuitable temperature or layer number. Changing conditions of printing can get different effects. And the bottom layer can not be easilypaste on the glass board below it, so glue is needed, don’t forget clear it after print.
QQ截图20150211154227.png
Views
Different views of the 3D model, it’s only 5cm tall but consist of more than 100 layers and spent more than 4 hours. Not so fast but i think it’s cheaper and more convenient, than any other ways to get this 3D model. By the way, I purchased the 3D-printer from Geeetech: http://www.geeetech.com/acrylic-geeetec ... p-884.html ,it’s suitable for beginners like me.
You do not have the required permissions to view the files attached to this post.
By fireworksfun
#179758
It's really a cheap 3D printer, I just want to make some 3D models, so i'm looking for one with poor budget :? . Is it easy to assemble?
By wenganxiang
#179795
fireworksfun wrote:It's really a cheap 3D printer, I just want to make some 3D models, so i'm looking for one with poor budget :? . Is it easy to assemble?
It's not so hard to assemble. For the machanical idiot like me, I spent about 3hours.
By Mee_n_Mac
#179800
wenganxiang wrote:
fireworksfun wrote:It's really a cheap 3D printer, I just want to make some 3D models, so i'm looking for one with poor budget :? . Is it easy to assemble?
It's not so hard to assemble. For the machanical idiot like me, I spent about 3hours.
As time goes by please post (I'm not sure where) your good and bad experiences. $300 is cheap, if it's all-inclusive. How much more (if any) would you it cost you to make 5 simple prints ? What's your guess as to cost/print/cm^3 (when you get a chance) ? An entry level printer can't be expected to 'compete' with a $3k one. How long does it take to make a print (perhaps some 'standard' print needs to be stated) ? How "rough" is the finished print (this is somewhat subjective) ?