SparkFun Forums 

Where electronics enthusiasts find answers.

General MicroView Support area - You have questions, find your answers here.

Moderators: Help@GeekAmmo, marcus@geekammo

By povezi
#175584
Are digital pins 5V (as std Arduino) or are the 3.3V?

I am thinking of interfacing with raspberry Pi GPIO and I probably need logic level shifter? :doh:
User avatar
By Ross Robotics
#175590
It's 5V logic. With all the information about the microview, I am astonished that there is no mention of it's logic level.. I looked for over 10 min and finally found it by reading the comments from the Kickstarter page.

I am glad I didn't buy one, as I find that there is a lot of info missing for doing real work with this device.
User avatar
By Ross Robotics
#175598
I recommend this one, https://www.sparkfun.com/products/12009

This one doesn't have an IC that could get damaged just by touching it..
By scotta
#175610
povezi wrote:Here is the converter http://www.dx.com/p/mini-rs232-to-ttl-c ... -5v-132934
That is not a 3.3V to 5V level shifter. It's a logic level to RS232 level shifter. The logic side levels can range from 3V to 5V. The other side will be RS232 levels (between +/- 5V and +/- 25V).

There's a good chance that you will fry your Raspberry Pi if you try to use it with this converter!
By awardblvr
#176229
The thing I like about these is that they also have a little voltage regulator for 3.3V so that you can power your 3.3V devices directly through this board.

I2C Logic Level Converter Bi-Directional Module 5V to 3.3V For Arduino BSS138 http://r.ebay.com/dd9r2n

5V-3V IIC UART SPI 4 Channel TTL Level Converter Adapter Module For Arduino 6Pin http://r.ebay.com/1KcJWp

There are several others as well... Not sure if Sparkfun has one with the built-in VR. But, It sure makes simple, low-current projects easy.