SparkFun Forums 

Where electronics enthusiasts find answers.

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!
#201372
Dear project people,I am an artist who is working on a project for an upcoming show. First, I would like to say I am a super n00b and would like to apologize for my ignorance The project I am working on makes use of HC-SR04 ultrasonic sensors and people moving. At the moment the sensors trigger a keyboard I have set-up in REAPER. When the viewer activates the sensor it triggers a sound. I have a code that works great for one sensor but I will eventually need to wire up 6-10 (sensors). I am unclear on how to make that happen. This is the code I am using at the moment.


#include <MIDI.h>
MIDI_CREATE_DEFAULT_INSTANCE();

int pingPin = 13;
int inPin = 12;
long duration;
int cm_new = 20;
int cm_old = 20;
int sens = 5; // sensivity range when to launch a new note

void setup() {

Serial.begin(9600); // MIDI Begin
pinMode(pingPin, OUTPUT); // setup the Pins
pinMode(inPin, INPUT); // setup the Pins

}

void loop()
{


// The PING is triggered by a HIGH pulse of 2 or more microseconds.
// Give a short LOW pulse beforehand to ensure a clean HIGH pulse:

digitalWrite(pingPin, LOW);
delayMicroseconds(2);
digitalWrite(pingPin, HIGH);
delayMicroseconds(10);
digitalWrite(pingPin, LOW);
duration = pulseIn(inPin, HIGH); // the singal from the Sensor is measured. The length of the pulse describes the distance form an object to the sensor.

cm_new = map(constrain(duration, 20, 3000), 50, 2000, 96, 48); // contrain --> set a threshold to cut values of the sensor that are to far away of to short (20 .. 3000) MAP --> Map the sensor range to a note values vom 96 (A high C) to 48 (a low C)

if (cm_new != cm_old) // only if a new sensor value is detected, a new note will be send. IF the object stays stable infront of the sensor, no note will be send.
{
MIDI.sendNoteOff(cm_old,0,1); // Stop the old note
MIDI.sendNoteOn(cm_new,127,1); // Send a new Note (pitch , velocity 127, on channel 1)
cm_old = cm_new;
}
delay(30); // for staiblity
}




I have also attached a pic to see what I'm up to… https://www.instagram.com/p/BrNvEtmn3Va ... hare_sheet

Not sure what changes are needed in the code. Help would be very appreciated appreciated!
I can even show you a video of the show once it's up!
Thanks for your time and help!
#201373
Cool project! Please use code tags ("</>" button) to post code, so that it looks like this:
Code: Select all
digitalWrite(pingPin, LOW);
delayMicroseconds(2);
digitalWrite(pingPin, HIGH);
delayMicroseconds(10);
digitalWrite(pingPin, LOW);
duration = pulseIn(inPin, HIGH); // the singal from the Sensor is measured. The length of the pulse describes the distance form an object to the sensor.
For each sonar sensor, you have to repeat the above, with each sensor ping and input connected to different pins, obviously. The sensors must be fired sequentially, with a few milliseconds delay between each sensor action. Otherwise the sensors (along with possible multiple sound reflections) will interfere with each other. With several sensors, you will need to adjust that delay time to minimize sensor cross talk, and may find that the overall ranging cycle is so slow as to be impractical.

You might consider instead using optical time of flight distance sensors, like the VL53L0X, which are much faster, quite directional and usually do not interfere with each other. See https://www.pololu.com/product/2490
long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]