Tsunami Super Wav Trigger - Can't get it to make sound

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!

Moderator: phalanx

Post Reply
ryurkovich
Posts: 28
Joined: Wed Mar 28, 2018 7:46 am

Tsunami Super Wav Trigger - Can't get it to make sound

Post by ryurkovich » Wed Nov 14, 2018 9:10 am

Hello,

I am trying to set up a Tsunami Super Wav player to play 5 different tracks of bird songs for a museum exhibit. Visitors would push a button and the corresponding individual speakers would play that track. Ideally the track won't be able to be started again until it is finished playing.

See proposed schematic:
Image

I am using this amp, and 8 ohm speakers, and a 5V 2A Micro USB Charger Power Adapter.
Dayton Audio DTA-1 Class D AC/DC Battery Powered Mini Amplifier 15 WPC
https://www.parts-express.com/dayton-au ... c--300-380

I read all of the instructions I could find, formatted the audio files to .wav, 44.1kHz, 16-bit, mono files.
They are titled as 001_A, 002_B, etc.
I loaded the most recent mono firmware on the sd card.
I loaded the .ini file on the sd card (See image)
Image

I haven't installed this with the long speaker wires yet, and am testing it with short ones.
When I connect the ground and + of the triggers, the audio doesn't seem to go through to the output 1.
The status light blinks once quickly every few seconds.
Is there anything I may be missing?
Thanks!

-Rachel
Attachments
Screen shot.png
Proposed Schematic Tsunami Player.jpg

robertsonics
Posts: 257
Joined: Fri Mar 24, 2006 7:58 am

Re: Tsunami Super Wav Trigger - Can't get it to make sound

Post by robertsonics » Wed Nov 14, 2018 2:17 pm

Have you gone step-by-step through the hookup guide?

ryurkovich
Posts: 28
Joined: Wed Mar 28, 2018 7:46 am

Re: Tsunami Super Wav Trigger - Can't get it to make sound

Post by ryurkovich » Thu Nov 15, 2018 9:33 am

Yes, I did..
I think it may be the file type. Even though I followed the right specs for exporting in Audition, It worked after exporting from Audacity.

ryurkovich
Posts: 28
Joined: Wed Mar 28, 2018 7:46 am

Re: Tsunami Super Wav Trigger - Can't get it to make sound

Post by ryurkovich » Fri Dec 07, 2018 8:55 am

Hello,

I have resolve the audio issue, it was the file type.

I now have a new issue I could use some help with.
Button input "E" which has a long cord running through the ceiling has been getting some interference and triggering the player automatically when the button isn't pushed. Is there any way to adjust settings / add resistors to the cord or board without running a whole new wire?

Someone suggested to me - "Adding a capacitor across the switch wires could help but this should probably be checked with Robertson to make sure that is compatible with the input. A capacitor can cut down the noise ripple voltage. " Is this possible, if so how?

Thanks

ryurkovich
Posts: 28
Joined: Wed Mar 28, 2018 7:46 am

Re: Tsunami Super Wav Trigger - Can't get it to make sound

Post by ryurkovich » Thu Dec 13, 2018 1:17 pm

We fixed this issue by adding a 0.047k uF capacitor straddled between the two button wires close to the board.

Post Reply