Bad characters while communication over serial port
Posted: Thu Sep 20, 2018 5:04 am
Hello All,
I am interfacing a SIM800 GSM module with Pi 3 over serial ports (pins 6, 8, 10). While things work OK most of the time, every now and then I get spurious characters in the response. For example, I get:
['+CLCC: 1,0,2,0,0,"+919812x\x9c\xd3\x13\x93\x93\x12)\xa25,""', 'OK']
whereas the expected response is: ['+CLCC: 1,0,2,0,0,"+919812012321,""', 'OK']
As I said, this happens once in a while (may be 1 in 10) and happens with other commands too. Also, this is not the only GSM module or Pi having the problem. So very unlikely hardware issue, unless the GSM module is buggy. The GSM module in question is this http://www.rhydolabz.com/wiki/?p=10450
The baudrate is set to 9600.
What could be going wrong? Could it be bad connections? I usually crimp dupont connectors to the open ends of the cable supplied with the modem. As far as I can tell, the crimps are decently done. How do I fix this?
Thanks,
Pavan
I am interfacing a SIM800 GSM module with Pi 3 over serial ports (pins 6, 8, 10). While things work OK most of the time, every now and then I get spurious characters in the response. For example, I get:
['+CLCC: 1,0,2,0,0,"+919812x\x9c\xd3\x13\x93\x93\x12)\xa25,""', 'OK']
whereas the expected response is: ['+CLCC: 1,0,2,0,0,"+919812012321,""', 'OK']
As I said, this happens once in a while (may be 1 in 10) and happens with other commands too. Also, this is not the only GSM module or Pi having the problem. So very unlikely hardware issue, unless the GSM module is buggy. The GSM module in question is this http://www.rhydolabz.com/wiki/?p=10450
The baudrate is set to 9600.
What could be going wrong? Could it be bad connections? I usually crimp dupont connectors to the open ends of the cable supplied with the modem. As far as I can tell, the crimps are decently done. How do I fix this?
Thanks,
Pavan