- Tue Sep 11, 2018 8:51 am
#200291
Hello!
Need some brainstorming help with this one.
Im making a circuit that will be attached to a boot, and simply flash bright like a camera flash. it should flash when the person stomps.
1 - Can the WakeonShake board handle a force like a stomp.. and not wake on regular steps? The datasheet says I can adjust the threshold, but were
not talking tapping the glass of a display..I see it can handle up to "+8g"
2 - I can settle for bright white LEDs, Or should I use a 12V LED
3 - I see the max voltage the WoS can output is 15v that should be enough. Does the WoS truly output a max of 15V?
4 - When I connect the WoS to a computer via the serial/USB hookup, do I need a certain software to edit the code?
Most of all, is this a good circut idea for this installation? Maybe someone else has a better idea?
-Sonny
Need some brainstorming help with this one.
Im making a circuit that will be attached to a boot, and simply flash bright like a camera flash. it should flash when the person stomps.
1 - Can the WakeonShake board handle a force like a stomp.. and not wake on regular steps? The datasheet says I can adjust the threshold, but were
not talking tapping the glass of a display..I see it can handle up to "+8g"
2 - I can settle for bright white LEDs, Or should I use a 12V LED
3 - I see the max voltage the WoS can output is 15v that should be enough. Does the WoS truly output a max of 15V?
4 - When I connect the WoS to a computer via the serial/USB hookup, do I need a certain software to edit the code?
Most of all, is this a good circut idea for this installation? Maybe someone else has a better idea?
-Sonny