SparkFun Forums 

Where electronics enthusiasts find answers.

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!
By Max771662
#200248
Hi, I couldn't find the exact answer to my question on the forum after digging for days so I thought I should ask it directly.
I have made my own Arduino UNO board for a small project and I am struggling with the USB functionality to upload sketches. I have designed my board using the ATMEGA328P and the ATMEGA16U2 in the exact same way than on an Arduino UNO board, the only differences with the UNO board are on the 328 I/O which are broken out in a different way (I have included the CAN shield directly on the board as well).

I bought as well an AVR programmer as I thought I will use it to program first both chip for the board to be recognized as an UNO through the IDE.

I have access to both ICSP header (one for the 328, one for the 16U) and I think I have loaded both bootloader. The all board is now recognized as 'Arduino UNO' when I connect the USB from the 16U2, which I think at least means that the 16U2 is correctly programmed. However, I cannot send any sketch through the IDE as it timeout with a "avrdude: stk500_recv(): programmer is not responding".

If I connect through the 328 ICSP header and use the 'Upload Using a Programmer' option, it works fine all functionalities are behaving as expected.

I think the only thing not working is the connection between the 328 and 16U when trying to load a sketch through USB, but not sure why? (wrong bootloader, wrong init...). On the circuitry I have kept as it is on an UNO all quartz, resistors, links, so I'm not sure if I missed something software-wise to declare both chips..

If anyone have a starting point or could guide towards something I would appreciate it massively!

Max
By machino
#201425
I dont know why are you using Atmega16u2 and why you need a AVR programmer to program self made arduino.
Its very easy to build arduino on breadboard, you just need Atmega328 IC, a crystal, few capacitors and resistors.
First you have to Burn Arduino boot loader into Atmega328 IC and then make the complete circuitry no breadboard or perfboard.
Then finally to program the arduino use USB to serial FTDI module, you will be able to program it with ARduino IDE same like Arduino.
THere are many online tutorials online to build it, the complete Arduino on breadboard will look like this
Image
Image source is https://circuitdigest.com/microcontroll ... rduino-ide, also find complete explanation there
long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]