- Fri Mar 16, 2018 5:33 pm
#198681
I'm sure is a simple matter for most here. This is my first time using Arduino and I haven't been able to find the specific answer to my problem so any help would be appreciated.
I need an arcade type momentary push button to turn on two different motors, both 125 volt, for a different period of time for each and then turn off until the next time the button is pushed. So, a person pushes the button, releases 1/2 second later. When they push, both motors turn on at the same time and then one runs for 10 seconds and the other runs for 12 seconds. Then they both turn off and stay off until the button is pushed again, so there is no repetition.
I have the 12v illuminated arcade switch, an Arduino uno, a relay. I've found plenty of debounce programs. I've found information on switches that, when pushed turn on an led and when pushed again, turn it off, and switches that will power the led as long as the button is held. But I haven't found anything about a switch that, when pushed for any amount of time, sets the above process into motion. Arduino code and wiring help would be great. For example, to wire the switch do I need to make a circuit that begins and ends in the Arduino, except for the illumination of the led in the switch?
I need an arcade type momentary push button to turn on two different motors, both 125 volt, for a different period of time for each and then turn off until the next time the button is pushed. So, a person pushes the button, releases 1/2 second later. When they push, both motors turn on at the same time and then one runs for 10 seconds and the other runs for 12 seconds. Then they both turn off and stay off until the button is pushed again, so there is no repetition.
I have the 12v illuminated arcade switch, an Arduino uno, a relay. I've found plenty of debounce programs. I've found information on switches that, when pushed turn on an led and when pushed again, turn it off, and switches that will power the led as long as the button is held. But I haven't found anything about a switch that, when pushed for any amount of time, sets the above process into motion. Arduino code and wiring help would be great. For example, to wire the switch do I need to make a circuit that begins and ends in the Arduino, except for the illumination of the led in the switch?