- Fri Feb 23, 2018 10:32 pm
#198469
Hello Arduino gurus,
I know nothing about Arduino. Going at this blindly. I truly envy you guys. This is some hard stuff. I asked for help at another forum but they needed to get paid which I find very strange. This is a hobby. Forums are places to get help.
I am looking to build a YouTube subscriber counter.
I have watched a very fasted paced tutorial video from www.educ8s.tv on how to create your very own YouTube subscriber counter display.
I have started the return process of my 20x4 display as I believe it to be DOA. I can't get any output to it or turn on the back light. The location is at 0x3F for the display, I checked to make sure.
I just need to program the ESP8266 D1 Mini and output to the 20x4 I2C LCD display.
These are the libraries I need. I believe I have added them successfully. The top three are in red, not sure why.
#include <Wire.h>
#include <ESP8266WiFi.h>
#include <LiquidCrystal_I2C.h>
#include <ArduinoJson.h>
If I get this working, I will give you a shout out in my Youtube video on who has helped me and direct everyone with a Arduino issue to come see ABC person(s). My channel is about reviews and how tos. I'm not trying to pass this off as my idea, but offer them a better tutorial making it easier for the beginner like myself.
Please tell me what I need to change or add to get this to work. Please let me know of this works for you and let me know what I need to do on my end to get it to work. where to download the correct libraries. Thank you.
JoeteckTips
Here is the code:
<begin code>
//////////////////////////////////////////////
// 20x4 Subscriber Counter for YouTube //
// //
// http://www.educ8s.tv //
/////////////////////////////////////////////
#include <Wire.h>
#include <ESP8266WiFi.h>
#include <LiquidCrystal_I2C.h>
#include <ArduinoJson.h>
byte LT[8] =
{
B01111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111
};
byte UB[8] =
{
B11111,
B11111,
B11111,
B00000,
B00000,
B00000,
B00000,
B00000
};
byte RT[8] =
{
B11110,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111
};
byte LL[8] =
{
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B01111
};
byte LB[8] =
{
B00000,
B00000,
B00000,
B00000,
B00000,
B11111,
B11111,
B11111
};
byte LR[8] =
{
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11110
};
byte UMB[8] =
{
B11111,
B11111,
B11111,
B00000,
B00000,
B00000,
B11111,
B11111
};
byte LMB[8] =
{
B11111,
B00000,
B00000,
B00000,
B00000,
B11111,
B11111,
B11111
};
const char* ssid = "SSID of local network"; // SSID of local network
const char* password = "Password on network"; // Password on network
String apiKey = "YouTube Data API"; // YouTube Data API v3 key generated here: // https://console.developers.google.com
String channelId = "YouTube channel id"; // YouTube channel id
const char *host = "www.googleapis.com";
long subscribers,subscribersBefore = 0;
LiquidCrystal_I2C lcd(0x3F, 2, 1, 0, 4, 5, 6, 7, 3, POSITIVE); // Set the LCD I2C address
void setup()
{
Serial.begin(9600);
int cursorPosition=0;
lcd.begin(20,4);
lcd.setCursor(0,0);
lcd.print("Connecting ....");
createCustomChars();
WiFi.begin(ssid, password);
while (WiFi.status() != WL_CONNECTED) {
delay(500);
lcd.setCursor(cursorPosition,1);
lcd.print(".");
cursorPosition++;
}
lcd.clear();
lcd.setCursor(0,0);
lcd.print("Connected!");
delay(1000);
}
void loop()
{
int length;
String subscribersString = String(getSubscribers());
if(subscribers != subscribersBefore)
{
lcd.clear();
length = subscribersString.length();
printSubscribers(length,subscribersString);
subscribersBefore = subscribers;
}
delay(60000);
}
void printSubscribers(int length, String subscribersString)
{
switch(length)
{
case 5: printDigits(subscribersString,5);printDigits(subscribersString,4);printDigits(subscribersString,3);printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 4: printDigits(subscribersString,4);printDigits(subscribersString,3);printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 3: printDigits(subscribersString,3);printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 2: printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 1: printDigits(subscribersString,1);break;
default: break;
}
}
void printDigits(String subscribersString,int digit)
{
int length = subscribersString.length();
char digitToPrint = subscribersString.charAt(length-digit);
Serial.println(digitToPrint);
switch(digit)
{
case 1: printDigitToScreen(digitToPrint,17); break;
case 2: printDigitToScreen(digitToPrint,13); break;
case 3: printDigitToScreen(digitToPrint,9); break;
case 4: printDigitToScreen(digitToPrint,5); break;
case 5: printDigitToScreen(digitToPrint,1); break;
}
}
void printDigitToScreen(char digit,int position)
{
int digitToPrint = digit - '0'; //Convertion from char to int
switch(digitToPrint)
{
case 1:digit1(position); break;
case 2:digit2(position); break;
case 3:digit3(position); break;
case 4:digit4(position); break;
case 5:digit5(position); break;
case 6:digit6(position); break;
case 7:digit7(position); break;
case 8:digit8(position); break;
case 9:digit9(position); break;
case 0:digit0(position); break;
}
}
void digit0(int position_x)
{
lcd.setCursor(position_x, 1);
lcd.write((byte)0);
lcd.write(1);
lcd.write(2);
lcd.setCursor(position_x, 2);
lcd.write(3);
lcd.write(4);
lcd.write(5);
}
void digit1(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(1);
lcd.write(2);
lcd.setCursor(position_x+1,2);
lcd.write(5);
}
void digit2(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(6);
lcd.write(6);
lcd.write(2);
lcd.setCursor(position_x, 2);
lcd.write(3);
lcd.write(7);
lcd.write(7);
}
void digit3(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(6);
lcd.write(6);
lcd.write(2);
lcd.setCursor(position_x,2);
lcd.write(7);
lcd.write(7);
lcd.write(5);
}
void digit4(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(3);
lcd.write(4);
lcd.write(2);
lcd.setCursor(position_x+2,2);
lcd.write(5);
}
void digit5(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write(6);
lcd.write(6);
lcd.setCursor(position_x,2);
lcd.write(7);
lcd.write(7);
lcd.write(5);
}
void digit6(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write(6);
lcd.write(6);
lcd.setCursor(position_x,2);
lcd.write(3);
lcd.write(7);
lcd.write(5);
}
void digit7(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(1);
lcd.write(1);
lcd.write(2);
lcd.setCursor(position_x+1,2);
lcd.write((byte)0);
}
void digit8(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write((byte)6);
lcd.write(2);
lcd.setCursor(position_x,2);
lcd.write(3);
lcd.write(7);
lcd.write(5);
}
void digit9(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write((byte)6);
lcd.write((byte)2);
lcd.setCursor(position_x+2,2);
lcd.write((byte)5);
}
int getSubscribers()
{
WiFiClientSecure client;
Serial.print("connecting to "); Serial.println(host);
if (!client.connect(host, 443)) {
Serial.println("connection failed");
return -1;
}
String cmd = String("GET /youtube/v3/channels?part=statistics&id=") + channelId + "&key=" + apiKey+ " HTTP/1.1\r\n" +
"Host: " + host + "\r\nUser-Agent: ESP8266/1.1\r\nConnection: close\r\n\r\n";
client.print(cmd);
int repeatCounter = 10;
while (!client.available() && repeatCounter--) {
delay(500);
}
String line,buf="";
int startJson=0;
while (client.connected() && client.available()) {
line = client.readStringUntil('\n');
if(line[0]=='{') startJson=1;
if(startJson)
{
for(int i=0;i<line.length();i++)
if(line=='[' || line==']') line=' ';
buf+=line+"\n";
}
}
client.stop();
DynamicJsonBuffer jsonBuf;
JsonObject &root = jsonBuf.parseObject(buf);
if (!root.success()) {
Serial.println("parseObject() failed");
delay(10);
return -1;
}
subscribers = root["items"]["statistics"]["subscriberCount"];
Serial.println(subscribers);
return subscribers;
}
void createCustomChars()
{
lcd.createChar(0,LT);
lcd.createChar(1,UB);
lcd.createChar(2,RT);
lcd.createChar(3,LL);
lcd.createChar(4,LB);
lcd.createChar(5,LR);
lcd.createChar(6,UMB);
lcd.createChar(7,LMB);
}
<end code>
I know nothing about Arduino. Going at this blindly. I truly envy you guys. This is some hard stuff. I asked for help at another forum but they needed to get paid which I find very strange. This is a hobby. Forums are places to get help.
I am looking to build a YouTube subscriber counter.
I have watched a very fasted paced tutorial video from www.educ8s.tv on how to create your very own YouTube subscriber counter display.
I have started the return process of my 20x4 display as I believe it to be DOA. I can't get any output to it or turn on the back light. The location is at 0x3F for the display, I checked to make sure.
I just need to program the ESP8266 D1 Mini and output to the 20x4 I2C LCD display.
These are the libraries I need. I believe I have added them successfully. The top three are in red, not sure why.
#include <Wire.h>
#include <ESP8266WiFi.h>
#include <LiquidCrystal_I2C.h>
#include <ArduinoJson.h>
If I get this working, I will give you a shout out in my Youtube video on who has helped me and direct everyone with a Arduino issue to come see ABC person(s). My channel is about reviews and how tos. I'm not trying to pass this off as my idea, but offer them a better tutorial making it easier for the beginner like myself.
Please tell me what I need to change or add to get this to work. Please let me know of this works for you and let me know what I need to do on my end to get it to work. where to download the correct libraries. Thank you.
JoeteckTips
Here is the code:
<begin code>
//////////////////////////////////////////////
// 20x4 Subscriber Counter for YouTube //
// //
// http://www.educ8s.tv //
/////////////////////////////////////////////
#include <Wire.h>
#include <ESP8266WiFi.h>
#include <LiquidCrystal_I2C.h>
#include <ArduinoJson.h>
byte LT[8] =
{
B01111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111
};
byte UB[8] =
{
B11111,
B11111,
B11111,
B00000,
B00000,
B00000,
B00000,
B00000
};
byte RT[8] =
{
B11110,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111
};
byte LL[8] =
{
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B01111
};
byte LB[8] =
{
B00000,
B00000,
B00000,
B00000,
B00000,
B11111,
B11111,
B11111
};
byte LR[8] =
{
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11111,
B11110
};
byte UMB[8] =
{
B11111,
B11111,
B11111,
B00000,
B00000,
B00000,
B11111,
B11111
};
byte LMB[8] =
{
B11111,
B00000,
B00000,
B00000,
B00000,
B11111,
B11111,
B11111
};
const char* ssid = "SSID of local network"; // SSID of local network
const char* password = "Password on network"; // Password on network
String apiKey = "YouTube Data API"; // YouTube Data API v3 key generated here: // https://console.developers.google.com
String channelId = "YouTube channel id"; // YouTube channel id
const char *host = "www.googleapis.com";
long subscribers,subscribersBefore = 0;
LiquidCrystal_I2C lcd(0x3F, 2, 1, 0, 4, 5, 6, 7, 3, POSITIVE); // Set the LCD I2C address
void setup()
{
Serial.begin(9600);
int cursorPosition=0;
lcd.begin(20,4);
lcd.setCursor(0,0);
lcd.print("Connecting ....");
createCustomChars();
WiFi.begin(ssid, password);
while (WiFi.status() != WL_CONNECTED) {
delay(500);
lcd.setCursor(cursorPosition,1);
lcd.print(".");
cursorPosition++;
}
lcd.clear();
lcd.setCursor(0,0);
lcd.print("Connected!");
delay(1000);
}
void loop()
{
int length;
String subscribersString = String(getSubscribers());
if(subscribers != subscribersBefore)
{
lcd.clear();
length = subscribersString.length();
printSubscribers(length,subscribersString);
subscribersBefore = subscribers;
}
delay(60000);
}
void printSubscribers(int length, String subscribersString)
{
switch(length)
{
case 5: printDigits(subscribersString,5);printDigits(subscribersString,4);printDigits(subscribersString,3);printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 4: printDigits(subscribersString,4);printDigits(subscribersString,3);printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 3: printDigits(subscribersString,3);printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 2: printDigits(subscribersString,2);printDigits(subscribersString,1);break;
case 1: printDigits(subscribersString,1);break;
default: break;
}
}
void printDigits(String subscribersString,int digit)
{
int length = subscribersString.length();
char digitToPrint = subscribersString.charAt(length-digit);
Serial.println(digitToPrint);
switch(digit)
{
case 1: printDigitToScreen(digitToPrint,17); break;
case 2: printDigitToScreen(digitToPrint,13); break;
case 3: printDigitToScreen(digitToPrint,9); break;
case 4: printDigitToScreen(digitToPrint,5); break;
case 5: printDigitToScreen(digitToPrint,1); break;
}
}
void printDigitToScreen(char digit,int position)
{
int digitToPrint = digit - '0'; //Convertion from char to int
switch(digitToPrint)
{
case 1:digit1(position); break;
case 2:digit2(position); break;
case 3:digit3(position); break;
case 4:digit4(position); break;
case 5:digit5(position); break;
case 6:digit6(position); break;
case 7:digit7(position); break;
case 8:digit8(position); break;
case 9:digit9(position); break;
case 0:digit0(position); break;
}
}
void digit0(int position_x)
{
lcd.setCursor(position_x, 1);
lcd.write((byte)0);
lcd.write(1);
lcd.write(2);
lcd.setCursor(position_x, 2);
lcd.write(3);
lcd.write(4);
lcd.write(5);
}
void digit1(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(1);
lcd.write(2);
lcd.setCursor(position_x+1,2);
lcd.write(5);
}
void digit2(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(6);
lcd.write(6);
lcd.write(2);
lcd.setCursor(position_x, 2);
lcd.write(3);
lcd.write(7);
lcd.write(7);
}
void digit3(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(6);
lcd.write(6);
lcd.write(2);
lcd.setCursor(position_x,2);
lcd.write(7);
lcd.write(7);
lcd.write(5);
}
void digit4(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(3);
lcd.write(4);
lcd.write(2);
lcd.setCursor(position_x+2,2);
lcd.write(5);
}
void digit5(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write(6);
lcd.write(6);
lcd.setCursor(position_x,2);
lcd.write(7);
lcd.write(7);
lcd.write(5);
}
void digit6(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write(6);
lcd.write(6);
lcd.setCursor(position_x,2);
lcd.write(3);
lcd.write(7);
lcd.write(5);
}
void digit7(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write(1);
lcd.write(1);
lcd.write(2);
lcd.setCursor(position_x+1,2);
lcd.write((byte)0);
}
void digit8(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write((byte)6);
lcd.write(2);
lcd.setCursor(position_x,2);
lcd.write(3);
lcd.write(7);
lcd.write(5);
}
void digit9(int position_x)
{
lcd.setCursor(position_x,1);
lcd.write((byte)0);
lcd.write((byte)6);
lcd.write((byte)2);
lcd.setCursor(position_x+2,2);
lcd.write((byte)5);
}
int getSubscribers()
{
WiFiClientSecure client;
Serial.print("connecting to "); Serial.println(host);
if (!client.connect(host, 443)) {
Serial.println("connection failed");
return -1;
}
String cmd = String("GET /youtube/v3/channels?part=statistics&id=") + channelId + "&key=" + apiKey+ " HTTP/1.1\r\n" +
"Host: " + host + "\r\nUser-Agent: ESP8266/1.1\r\nConnection: close\r\n\r\n";
client.print(cmd);
int repeatCounter = 10;
while (!client.available() && repeatCounter--) {
delay(500);
}
String line,buf="";
int startJson=0;
while (client.connected() && client.available()) {
line = client.readStringUntil('\n');
if(line[0]=='{') startJson=1;
if(startJson)
{
for(int i=0;i<line.length();i++)
if(line=='[' || line==']') line=' ';
buf+=line+"\n";
}
}
client.stop();
DynamicJsonBuffer jsonBuf;
JsonObject &root = jsonBuf.parseObject(buf);
if (!root.success()) {
Serial.println("parseObject() failed");
delay(10);
return -1;
}
subscribers = root["items"]["statistics"]["subscriberCount"];
Serial.println(subscribers);
return subscribers;
}
void createCustomChars()
{
lcd.createChar(0,LT);
lcd.createChar(1,UB);
lcd.createChar(2,RT);
lcd.createChar(3,LL);
lcd.createChar(4,LB);
lcd.createChar(5,LR);
lcd.createChar(6,UMB);
lcd.createChar(7,LMB);
}
<end code>