- Thu Jun 22, 2017 9:45 pm
#195278
Hi guys Ive been playing with a project that has a pir sensor and originally had a relay control and i have swapped it out for optocoupler to trigger a momentary push button to shutdown the pi I can get it to shut down but nothing comes back up on with the "button push" until i manually jump the pins on the pi I dont know if this is the right forum to post in but im just doing circles here is the code
Code: Select all
#include <FastLED.h>
/////////////////////////////
//VARS
//the time we give the sensor to calibrate (10-60 secs according to the datasheet)
int calibrationTime = 10;
//the time when the sensor outputs a low impulse
long unsigned int lowIn;
//the amount of milliseconds the sensor has to be low
//before we assume all motion has stopped
long unsigned int pause = 120000;
boolean lockLow = true;
boolean takeLowTime;
int pirPin = 2; //the digital pin connected to the PIR sensor's output
int relayPin = 4;
int buttonPin = 8;
#define MARQUEE_PIN 11
#define BACKLIGHT_PIN 12
#define COLOR_ORDER GRB
#define CHIPSET WS2812B
#define NUM_LEDS 150
#define initBRIGHTNESS 40
#define BRIGHTNESS 100
#define FRAMES_PER_SECOND 500
int MARQcolor = CRGB::White;
int BACKcolor = CRGB::Blue;
int lightState = 0; //0 off, 1, fading up, 2 on, 3 fading down
int fadeStep = 0;
int fadeStepSize = 2;
bool isAnimating = 0;
CRGB MARQ_leds[NUM_LEDS];
CRGB BL_leds[NUM_LEDS];
/////////////////////////////
//SETUP
void setup(){
Serial.begin(9600);
pinMode(buttonPin, INPUT);
pinMode(pirPin, INPUT);
pinMode(relayPin, OUTPUT);
pinMode(MARQUEE_PIN, OUTPUT);
pinMode(BACKLIGHT_PIN, OUTPUT);
digitalWrite(pirPin, LOW);
FastLED.addLeds<CHIPSET, BACKLIGHT_PIN, COLOR_ORDER>(BL_leds, NUM_LEDS).setCorrection( TypicalLEDStrip );
FastLED.addLeds<CHIPSET, MARQUEE_PIN, COLOR_ORDER>(MARQ_leds, NUM_LEDS).setCorrection( TypicalLEDStrip );
FastLED.setBrightness( initBRIGHTNESS );
if(digitalRead(buttonPin) == HIGH){
digitalWrite(relayPin,LOW);
for( int j = 0; j < 20; j++) {
MARQ_leds[j] = CRGB::Orange;
BL_leds[j] = CRGB::Orange;
}
setAllBrightNess(10);
FastLED.show();
//give the sensor some time to calibrate
Serial.print("calibrating sensor ");
for(int i = 0; i < calibrationTime; i++){
Serial.print(".");
delay(1000);
}
Serial.println(" done");
Serial.println("SENSOR ACTIVE");
setAllBrightNess(0);
delay(50);
} else {
digitalWrite(relayPin,HIGH);
}
}
////////////////////////////
//LOOP
void loop(){
if(digitalRead(buttonPin) == HIGH){
// turn on sensors
if(digitalRead(pirPin) == HIGH){
if(lockLow){
//makes sure we wait for a transition to LOW before any further output is made:
lockLow = false;
Serial.println("---");
Serial.print("motion detected at ");
Serial.print(millis()/1000);
Serial.println(" sec");
if(lightState != 2){
lightState = 1;
}
digitalWrite(relayPin,HIGH);
delay(50);
}
takeLowTime = true;
}
if(digitalRead(pirPin) == LOW){
if(takeLowTime){
lowIn = millis(); //save the time of the transition from high to LOW
takeLowTime = false; //make sure this is only done at the start of a LOW phase
}
//if the sensor is low for more than the given pause,
//we assume that no more motion is going to happen
if(!lockLow && millis() - lowIn > pause){
//makes sure this block of code is only executed again after
//a new motion sequence has been detected
lockLow = true;
Serial.print("motion ended at "); //output
Serial.print((millis() - pause)/1000);
Serial.println(" sec");
if(lightState != 0){
lightState= 3;
}
digitalWrite(relayPin,LOW);
FastLED.show();
delay(50);
}
}
switch(lightState){
case 0:
//light is off
break;
case 1:
//light is animating up
lightIsAnimatingUp();
break;
case 2:
//light is on
lightIsOn();
break;
case 3:
//light is animating down
lightIsAnimatingDown();
break;
}
FastLED.show(); // display this frame
} else {
//sensors are off.. just light up.
digitalWrite(relayPin,HIGH);
for( int j = 0; j < NUM_LEDS; j++) {
MARQ_leds[j] = MARQcolor;
BL_leds[j] = BACKcolor;
}
setAllBrightNess(BRIGHTNESS);
FastLED.show();
}
}
void setColors(){
for( int j = 0; j < NUM_LEDS; j++) {
MARQ_leds[j] = MARQcolor;
BL_leds[j] = BACKcolor;
}
}
void lightIsOn()
{
setColors();
delay(100);
}
void lightIsAnimatingUp(){
fadeStep+=fadeStepSize;
setColors();
setAllBrightNess(fadeStep);
Serial.println(fadeStep);
delay(50);
if (fadeStep == BRIGHTNESS){
isAnimating=0;
lightState = 2;
}
}
void lightIsAnimatingDown(){
fadeStep-=fadeStepSize;
setColors();
setAllBrightNess(fadeStep);
delay(50);
if (fadeStep == 0){
isAnimating=0;
lightState = 0;
}
}
int setAllBrightNess(int val){
FastLED.setBrightness( val );
}