- Fri Jun 16, 2017 1:06 am
#195201
1: Now, I am using Raspberry Pi with Ultrasonic HCSR 04 Sensor. I have written a program for that. I got a proper result, but I am facing some reliability issue with that. So I thought I will use other sensors.
Statement 2: I bought Maxbotics sensor MB 1040, but I don't know how to program. I have tried with the same ultrasonic program, I got readings but that is not proper reading, I have not achieved accuracy. I have written a program in C++. So kindly help me to solve this issue.
Here I have added my sample code, what I have tried. I hope here will get a solution.
Statement 2: I bought Maxbotics sensor MB 1040, but I don't know how to program. I have tried with the same ultrasonic program, I got readings but that is not proper reading, I have not achieved accuracy. I have written a program in C++. So kindly help me to solve this issue.
Here I have added my sample code, what I have tried. I hope here will get a solution.
Code: Select all
#define TRIGGER_SENSOR 7 // GPIO_7
#define ECHO_SENSOR 15 // GPIO_8
// Distance variable
uint32_t Start_Sensor=0,Stop_Sensor=0;
uint32_t Time_Diff_Sensor=0;
float Range_Sensor=0;
volatile int Flag_Sensor=0;
pinMode(TRIGGER_SENSOR,OUTPUT); // Pins assignment
pinMode(ECHO_SENSOR,INPUT);
pullUpDnControl(ECHO_SENSOR,PUD_DOWN);
float Sensor::SensorDistance() // Sonar function
{
Start_Sensor=0;
Stop_Sensor= 0;
Flag_Sensor= 0;
digitalWrite(TRIGGER_SENSOR,0);
delayMicroseconds(1);
digitalWrite(TRIGGER_SENSOR,1);
delayMicroseconds(10);
digitalWrite(TRIGGER_SENSOR,0);
return Range_Sensor;
}
void myInterruptSensor(void) // Interrupt routine for Sensor distance
{ // Called whenever the input pin toggles
uint32_t timeTempSensorultra=micros();
if(Flag_Sensor==0) // first toggle? note the time
{
Start_Sensor=timeTempSensorultra;
Flag_Sensor=1;
}
else // second toggle? compute the distance
{
Stop_Sensor=timeTempSensorultra;
Flag_Sensor=0;
Time_Diff_Sensor=Stop_Sensor-Start_Sensor;
Range_Sensor=Time_Diff_Sensor/58.;
}
}
bool Sensor::Interrupt_error()
{
if(wiringPiISR(ECHO_SENSOR,INT_EDGE_BOTH,&myInterruptSensor) < 0)
{
cerr<<"interrupt error ["<<strerror (errno)<< "]:"<<errno<<endl;
return false;
}
return true;
}