- Sun Jan 22, 2017 2:19 pm
#193017
Hi,
I'm building a simple project that measures the temperature in an automobile oil pan.
Input: thermister based temp sensor mounted to oil pan
Output: RGB LED who's color is based on temperature bands
Brains: Arduino Pro Mini on a 2.54mm pitch protoboard, contained in a small project box
I need to understand more about which connectors I can use- since this is automotive, connectors will be subject to vibration and temperature - project will be mounted on the interior of the car so outdoor weather resistance is not a concern.
I'm going to need 3 connections coming into my project box: Power (2 positions), Input (2 positions), Output (4 positions)
Originally I was thinking I would want to mount 3 connectors on the project box itself (ie cut a hole and mount a connector in the hole), and that I would also have connectors mounted to the protoboard as well.
At first I was looking at Molex SL and Molex KK254, but I don't see anything that would allow me to mount a connection in a hole on the project box. can someone help me out? I was hoping ot use the same family of connectors throughout but if that isn't possible I could probably use molex on the protoboard and something else mounted on the box...
thanks in advance
I'm building a simple project that measures the temperature in an automobile oil pan.
Input: thermister based temp sensor mounted to oil pan
Output: RGB LED who's color is based on temperature bands
Brains: Arduino Pro Mini on a 2.54mm pitch protoboard, contained in a small project box
I need to understand more about which connectors I can use- since this is automotive, connectors will be subject to vibration and temperature - project will be mounted on the interior of the car so outdoor weather resistance is not a concern.
I'm going to need 3 connections coming into my project box: Power (2 positions), Input (2 positions), Output (4 positions)
Originally I was thinking I would want to mount 3 connectors on the project box itself (ie cut a hole and mount a connector in the hole), and that I would also have connectors mounted to the protoboard as well.
At first I was looking at Molex SL and Molex KK254, but I don't see anything that would allow me to mount a connection in a hole on the project box. can someone help me out? I was hoping ot use the same family of connectors throughout but if that isn't possible I could probably use molex on the protoboard and something else mounted on the box...
thanks in advance