- Wed Jan 18, 2017 6:52 pm
#192966
Hi,
I'm hoping somebody maybe able to assist or point me in the right direction. I'm looking to create a small project that will read the ID of an rfid tag in close range < 40mm, note which of six analog inputs is live (only one will be at anyone time) then post the rfid value, together with a five digit pre-programmed number and a second single-digit number that correlates to the analog input to a web connected database.
Having originally thought of doing this with a pic processor, it occurred to me looking around the it should be possible using sparkfun kit. I enjoy programming, but have no idea when it comes to designing circuits. Can anyone tell me if the above is doable, and point me in the right direction as to how it could be achieved? It's only for a hobby project, but I'm keen to learn a bit more about circuits!
Rick
I'm hoping somebody maybe able to assist or point me in the right direction. I'm looking to create a small project that will read the ID of an rfid tag in close range < 40mm, note which of six analog inputs is live (only one will be at anyone time) then post the rfid value, together with a five digit pre-programmed number and a second single-digit number that correlates to the analog input to a web connected database.
Having originally thought of doing this with a pic processor, it occurred to me looking around the it should be possible using sparkfun kit. I enjoy programming, but have no idea when it comes to designing circuits. Can anyone tell me if the above is doable, and point me in the right direction as to how it could be achieved? It's only for a hobby project, but I'm keen to learn a bit more about circuits!
Rick