- Thu Dec 29, 2016 7:00 am
#192680
I have written the following sketch:
It works fine since by regulating the potentiometer I am getting different readouts like 0.00 up to 5.00 depending on the amount of resistance.
Now, I simply want to run this program on the Pro Micro 5V/16Mhz. I connected the potentiometer imo appropriately and and uploaded the sketch. However, in that case I am constantly getting something inbetween 0.94volt and 1.21volt independently of the setting of the potentiometer - it just varies randomly. So, I thought that I should remove the potentiometer. But, that did confuse me even more since the randomly varying measurements of 0.94volt and 1.21volt remain the same regardless of a connected potentiometer.
Anybody got an idea why this super simple setup works on Arduino Uno but not on the Pro Micro?
Code: Select all
At first I used my Arduino Uno with the following setup: https://www.arduino.cc/en/Tutorial/ReadAnalogVoltagevoid setup() {
Serial.begin(9600);
}
void loop() {
int sensorValue = analogRead(A0);
float voltage = sensorValue * (5.0 / 1023.0);
Serial.println(voltage);
delay(1000);
}
It works fine since by regulating the potentiometer I am getting different readouts like 0.00 up to 5.00 depending on the amount of resistance.
Now, I simply want to run this program on the Pro Micro 5V/16Mhz. I connected the potentiometer imo appropriately and and uploaded the sketch. However, in that case I am constantly getting something inbetween 0.94volt and 1.21volt independently of the setting of the potentiometer - it just varies randomly. So, I thought that I should remove the potentiometer. But, that did confuse me even more since the randomly varying measurements of 0.94volt and 1.21volt remain the same regardless of a connected potentiometer.
Anybody got an idea why this super simple setup works on Arduino Uno but not on the Pro Micro?