- Tue Sep 20, 2016 12:45 pm
#191754
Hi All,
I have spent most of my morning attempting to put together a simple 555 timer and Big Easy driver. I have encountered a problem. The stepper motor clicks one time when the whole circuit is powered up, and then locks the motor shaft. The 555 is sending pulses as I have an LED blinking away happily at about one per second. The Big Easy LED is shining nice and bright. When I disconnect the 555 output and tap that output lead from the 555 to the input lead on the BED the motor does step. I also attempted to use 2 555's to provide a distinct division between pulses and the results are the same. All I am trying to do is drive the stepper for a equatorial mount at a constant rpm for night sky photography, but obviously something is amiss. I would have thought simple pulses would suffice. I have used a 7805 on the 555 side and am powering the BED with a 12v wall wart of 1.5 Amp and its output is actually 11.6v DC. The motor is an Epson FM-257. Do I need a driver transistor on the 555 pulse, or a pulldown resistor on the 555 output? Thanks in advance for any advice.
I have spent most of my morning attempting to put together a simple 555 timer and Big Easy driver. I have encountered a problem. The stepper motor clicks one time when the whole circuit is powered up, and then locks the motor shaft. The 555 is sending pulses as I have an LED blinking away happily at about one per second. The Big Easy LED is shining nice and bright. When I disconnect the 555 output and tap that output lead from the 555 to the input lead on the BED the motor does step. I also attempted to use 2 555's to provide a distinct division between pulses and the results are the same. All I am trying to do is drive the stepper for a equatorial mount at a constant rpm for night sky photography, but obviously something is amiss. I would have thought simple pulses would suffice. I have used a 7805 on the 555 side and am powering the BED with a 12v wall wart of 1.5 Amp and its output is actually 11.6v DC. The motor is an Epson FM-257. Do I need a driver transistor on the 555 pulse, or a pulldown resistor on the 555 output? Thanks in advance for any advice.