- Mon Aug 25, 2014 1:30 pm
#174129
I need to obtain two voltages from a single input. One is to power the RAW pin on a Pro Micro 5V, and the other is to feed an ADC input.
The source of the voltage is a 12V (2x 6V in series) deep cycle battery. This will be using the battery power while the battery is under charge, so I expect it to vary from a low of 11.5V up to 15V. Both of those are outside conservative numbers, in reality I expect to see 11.8V - 14.8V.
From this I need to get a voltage to power the RAW pin (which is rated up to 12V). This was discussed at length in another thread last week, where it became obvious that anything over 12V was skating on thin ice. The other voltage is to feed one of the ADC pins, and allow me to read where the charge state is within the 11.5-15V range.
This is what I have come up with, and would like a bit of peer review to see if I am missing anything obvious. The value of R1 is still undetermined, but I suspect something between 500-1K will be a good choice.
The source of the voltage is a 12V (2x 6V in series) deep cycle battery. This will be using the battery power while the battery is under charge, so I expect it to vary from a low of 11.5V up to 15V. Both of those are outside conservative numbers, in reality I expect to see 11.8V - 14.8V.
From this I need to get a voltage to power the RAW pin (which is rated up to 12V). This was discussed at length in another thread last week, where it became obvious that anything over 12V was skating on thin ice. The other voltage is to feed one of the ADC pins, and allow me to read where the charge state is within the 11.5-15V range.
This is what I have come up with, and would like a bit of peer review to see if I am missing anything obvious. The value of R1 is still undetermined, but I suspect something between 500-1K will be a good choice.
You do not have the required permissions to view the files attached to this post.
First learned EE at the juncture of vacuum tubes and solid state, Still learning.