- Sat May 31, 2014 2:10 pm
#171583
I was looking at the ULN2803A to drive the displays on a counter I'm building. At first I thought that it was pretty clever turning a 3-pin component into a 2-pin component, but the more I thought about it, the less sense this made.
It wouldn't have worked in my case, since the 4026 chip outputs only .44mA at 5v, so each input alone wouldn't drive a single LED without a transistor, which was, BTW, the reason for looking at the 2803. I realized that all the 2803 would be is a complicated resistor. The input voltage and current is driving the gate and is coming out at a smaller current and voltage than it was when it went in, but otherwise going straight through. :think:
Why would I ever want to use a Darlington array? It *does* have a purpose, right?
It wouldn't have worked in my case, since the 4026 chip outputs only .44mA at 5v, so each input alone wouldn't drive a single LED without a transistor, which was, BTW, the reason for looking at the 2803. I realized that all the 2803 would be is a complicated resistor. The input voltage and current is driving the gate and is coming out at a smaller current and voltage than it was when it went in, but otherwise going straight through. :think:
Why would I ever want to use a Darlington array? It *does* have a purpose, right?